Hello there,
i want to generate a 8 MHz clock signal with Timer_A Module of the MSP432P401. It should have a duty cycle of 50%. My main clock comes from an 48 MHz crystal oscillator.
But with respect to the specs (Timer_A max Clock: 24MHz) I don't see any possible configuration to get the desired clock signal.
The only possibility i have found is a 8 MHz signal with 66,7% or 33,3% duty cycle.
I hope I am wrong, and you can help me...
Thanks and best regards