This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I'm trying to use the BSL_Scripter with a MSP-FET and a F5342 target. I have followed the reccomendations here:
http://e2e.ti.com/support/microcontrollers/msp430/f/166/p/391358/1579705
BSL_Scripter is v1.07 from slau319j, MSP-FET is updated to latest firmware from MSP430Flasher_1.3.7. Debug Stack/drivers on the win7 PC are the latest 3.05.01.01.
With PuTTY, I verified that the MSP-FET will generate the 'BSL entry' sequence, changing the baud rate works, and the backchannel UART functions correctly.
However, the CHANGE_BAUD_RATE generates a fail from BSL_Scripter, regardless of the parameter. After a failed attempt, I need to unplug/replug the USB cable to the MSP-FET to get it to work again.
Test script:
MODE 5xx COM8
VERBOSE
CHANGE_BAUD_RATE 19200
DELAY 100
I get the same 'FAIL' result with 9600, 9601, 9621, and 9620 parameters.
Thanks,
Tim
**Attention** This is a public forum