This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430Flasher whit s-record

Other Parts Discussed in Thread: MSP430F5324

Hi,

I need a firmware file in s-record format so I set the "Output Format Option" to motorola m=2 in "MSP430Hex Utility"(CCSv6).  I need also to program the MSP430f5324  in command line so I use a MSP430flasher bat it is not compatible with s-record format. I need to TI-TXT format for MSP430flasher.

Can I generate both  file (s-record and ti-txt) in one compile operation in CCSv6?

Thanks to all.

Thomas

**Attention** This is a public forum