Hi All,
I have designed a custom PCB with the MSP430FR5739 as the core microcontroller. My design is with respect to the design specifications on the MSP-EXP430FR5739 schematic, and I have been trying to program my custom PCB with the emulator of the MSP-EXP430FR5739 experiential board, but everytime I try to load a simple program like switching on 2 led's I get an error from the code composer studio such as this:
[ MSP430: Error connecting to the target: Could not find device (or device not supported) ]
I am able to program the experimental board (MSP-EXP430FR5739) on it's own, meaning that works well, but I can't use that emulator to program my custom PCB.
I have connected the SBW (Spy-Bi-Wire) configuration from the experimental board emulator (TEST, RST, GND & Vcc) to the custom PCB (MSP430FR5739) corresponding pins, yet I still encounter the same error message on my CCSv6.1.1.
I've verified that the power going into the custom PCB is: 3.56V on Vcc and 1.48V on VCore. Likewise, the only differences I can see between my schematic for my custom PCB, and experimenter board (MSP-EXP430FR5739) are slightly different capacitance values on VCore. I have a 0.1u capacitor on VCore instead of 470n on the experimenter board. Otherwise, as far as I can tell the schematics are the same.
Could someone assist me regarding this? is there something that I'm missing on this matter?
Regards,
Lubabalo