Other Parts Discussed in Thread: MSP430FR6989, MSP430FR5739
Hi,
we tried to executed the example below in order to write in FRAM. We use the CCS. At the end we read in the variable *FRAM_write_ptr the value = 0xFFFFFFFF, so it does't work
Our final goal is to store data coming from ADCs in FRAM (data logger).
Where is the mistake?
Is it the right way to proceed?
#include <msp430.h>
void FRAMWrite(void);
//unsigned char count = 0;
unsigned long *FRAM_write_ptr;
unsigned long data;
#define FRAM_TEST_START 0xD000
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
// Configure GPIO
P1OUT &= ~BIT0; // Clear P1.0 output latch for a defined power-on state
P1DIR |= BIT0; // Set P1.0 to output direction
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Initialize dummy data
data = 0x00010001;
while(1)
{
// data += 0x00010001;
FRAM_write_ptr = (unsigned long *)FRAM_TEST_START;
FRAMWrite(); // Endless loop
// count++;
// if (count > 100)
// {
// P1OUT ^= 0x01; // Toggle LED to show 512K bytes
// count = 0; // ..have been written
// data = 0x00010001;
// }
}
}
void FRAMWrite(void)
{
// unsigned int i=0;
// for ( i= 0; i<128; i++)
// {
*FRAM_write_ptr = data;
__no_operation();
// }
}