This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uart msp4305529

Other Parts Discussed in Thread: MSP-EXP430F5529LP

Dear sir,

I am trying with msp4305529 UART program,but i am not getting the output on hyperterminal.Please go throgh the attachment.

thank you

#include "msp430.h"
char data1[]={"lets play \r\n"};
char data2[]={"hello guys how are you \r\n"};
void uart_init( void )
{
   	  P3SEL |= BIT3+BIT4;                       // P3.3,4 = USCI_A0 TXD/RXD
	  UCA0CTL1 |= UCSWRST;                      // **Put state machine in reset**
	  UCA0CTL1 |= UCSSEL_2;                     // SMCLK
	  UCA0BR0 = 9;                              // 1MHz 115200 (see User's Guide)
	  UCA0BR1 = 0;                              // 1MHz 115200
	  UCA0MCTL |= UCBRS_1 + UCBRF_0;            // Modulation UCBRSx=1, UCBRFx=0
	  UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
	  UCA0IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt
}//Initialize USCI state machine

void uart_send_byte( unsigned char data )
{
while (!(UCA0IFG&UCTXIFG));             // USCI_A0 TX buffer ready?
UCA0TXBUF = data;//The transmit data buffer holds the data waiting to be moved into the transmit shift register
}
void main(void)
{
unsigned int i=0,j=0;
WDTCTL = WDTPW + WDTHOLD; // Stop Watchdog timer



uart_init();

while( 1 )
{
for (i=0; i<14; i++)
{
uart_send_byte( data1[i] );
}
for(j=0;j<25;j++)
{
uart_send_byte(data2[j]);

}
__bis_SR_register( LPM3_bits + GIE );
}
}

**Attention** This is a public forum