This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[MSP430G2553] DCO frequency settings

Guru 24520 points

Other Parts Discussed in Thread: MSP430G2553

HI TI Experts,

Please let me confirm the following question.

[Question]

Would you please teach me the register settings for DCO in order to run the 4MHz?

If you have any questions, please let me know.

Best regards.

Kaka

  • There are open source code examples for MSP430G2553

    http://www.ti.com/lit/zip/slac485

    And there is msp430g2xx3_dco_flashcal.c file inside zip, where any DCO you want can be stored in device.

    #define DELTA_1MHZ    244                   // 244 x 4096Hz = 999.4Hz
    #define DELTA_8MHZ    1953                  // 1953 x 4096Hz = 7.99MHz
    #define DELTA_12MHZ   2930                  // 2930 x 4096Hz = 12.00MHz
    #define DELTA_16MHZ   3906                  // 3906 x 4096Hz = 15.99MHz

  • Hi

    Thank you for your advice.
    I could run the MSP430G2553 with 4MHz.

    Best regards.
    Kaka

**Attention** This is a public forum