This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi, all. i got the adc14 sampling problem again .
i tried the adc sampling code( C code and driverlib code from TI) and found both results exceed my expection.
the C code is the single channel repeat mode and another is multi channels repeat mode
the difference between the max and min of raw data, which i got from ADC14MEM0, can be larger than 30 counts, even up to 70 counts.
why the noise level is so high??
someone helps!
the C code listed as follows
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2013, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP432 CODE EXAMPLE DISCLAIMER
*
* MSP432 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/.../mspdriverlib for an API functional
* library & https://dev.ti.com/pinmux/ for a GUI approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP432P401 Demo - ADC14, Repeated Sequence of Conversions
//
// Description: This example shows how to perform a repeated sequence of
// conversions using "repeat sequence-of-channels" mode. AVcc is used for the
// reference and repeated sequence of conversions is performed on Channels A0,
// A1, A2, and A3. Each conversion result is stored in ADC14MEM0, ADC14MEM1,
// ADC14MEM2, and ADC14MEM3 respectively. After each sequence, the 4 conversion
// results are moved to A0results[], A1results[], A2results[], and A3results[].
// Test by applying voltages to channels A0 - A3. Open a watch window in
// debugger and view the results. Set Breakpoint1 in the index increment line
// to see the array values change sequentially and Breakpoint2 to see the entire
// array of conversion results in A0results[], A1results[], A2results[], and
// A3results[]for the specified Num_of_Results.
//
// Note that a sequence has no restrictions on which channels are converted.
// For example, a valid sequence could be A0, A3, A2, A4, A2, A1, A0, and A7.
// See the User's Guide for instructions on using the ADC14.
//
// MSP432P401
// -----------------
// /|\| |
// | | |
// --|RST |
// | |
// Vin0 -->|P5.5/A0 |
// Vin1 -->|P5.4/A1 |
// Vin2 -->|P5.3/A2 |
// Vin3 -->|P5.2/A3 |
// | |
//
// Wei Zhao
// Texas Instruments Inc.
// June 2014
// Built with Code Composer Studio V6.0
//******************************************************************************
#include "msp.h"
#include <stdint.h>
#define Num_of_Results 8
volatile uint16_t A0results[Num_of_Results];
volatile uint16_t A1results[Num_of_Results];
volatile uint16_t A2results[Num_of_Results];
volatile uint16_t A3results[Num_of_Results];
static uint8_t index;
int main(void)
{
WDTCTL = WDTPW+WDTHOLD; // Stop watchdog timer
// Configure GPIO
P5SEL1 |= BIT5 | BIT4 | BIT3 |BIT2; // Enable A/D channel A0-A3
P5SEL0 |= BIT5 | BIT4 | BIT3 |BIT2;
__enable_interrupt();
NVIC_ISER0 = 1 << ((INT_ADC14 - 16) & 31);// Enable ADC interrupt in NVIC module
ADC14CTL0 = ADC14ON | ADC14MSC | ADC14SHT0__192 | ADC14SHP | ADC14CONSEQ_3; // Turn on ADC14, extend sampling time
// to avoid overflow of results
ADC14MCTL0 = ADC14INCH_0; // ref+=AVcc, channel = A0
ADC14MCTL1 = ADC14INCH_1; // ref+=AVcc, channel = A1
ADC14MCTL2 = ADC14INCH_2; // ref+=AVcc, channel = A2
ADC14MCTL3 = ADC14INCH_3+ADC14EOS; // ref+=AVcc, channel = A3, end seq.
ADC14IER0 = ADC14IE3; // Enable ADC14IFG.3
SCB_SCR &= ~SCB_SCR_SLEEPONEXIT; // Wake up on exit from ISR
while(1)
{
ADC14CTL0 |= ADC14ENC | ADC14SC; // Start conversion-software trigger
__sleep();
__no_operation(); // For debugger
}
}
// ADC14 interrupt service routine
void adc_isr(void)
{
if (ADC14IFGR0 & ADC14IFG3)
{
A0results[index] = ADC14MEM0; // Move A0 results, IFG is cleared
A1results[index] = ADC14MEM1; // Move A1 results, IFG is cleared
A2results[index] = ADC14MEM2; // Move A2 results, IFG is cleared
A3results[index] = ADC14MEM3; // Move A3 results, IFG is cleared
index = (index + 1) & 0x7; // Increment results index, modulo
__no_operation(); //Set Breakpoint1 here
}
}
void SysTick_ISR()
{
}
**Attention** This is a public forum