Hi,
Are MSP430F5659IPZR and MSP430F5335IPZR pin compatible (if we don't use the third USCI)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Are MSP430F5659IPZR and MSP430F5335IPZR pin compatible (if we don't use the third USCI)?
Hi Chee-Boon!
The easiest way to find out is comparing the datasheets of the MSP430F5659 and MSP430F5335. Both documents have one page that show the processor with it's pinout:
Beside from the important pins like power, reset, ... it of course depends on your application because the processors might have different functionality. So it is not possible to answer this question with a simple yes or no. For example look at the upper right corner of the devices and compare the pinout. Now look into the datasheet to see how these pins have to be connected and if the devices are replaceable.
Dennis
**Attention** This is a public forum