Hello everyone, I sent a question to AskTexas support and was advised to rise a topic here...
One of our designs is based on a MSP430FR6972 FRAM micro-controller as a CPU.
We ordered a couple of parts as samples at the end of 2015 and tested them in prototype boards.
Testing showed good results so we decided to put them into mass production and purchased 600 chips
from one of TI's official distributors.
After half of the PCB-s have been assembled we bumped into some peculiar problem with FRAM failing to be re-programmed.
All the processors were initially programmed OK, but some samples have one FRAM page failing to be reprogrammed.
Actually it fails to be erased, giving as a result array of 0xFF3F values instead of 0xFFFF for the erased state.
Now we already have 3 parts failing out of 3 taken for experiments with program code improvement. One of them ceased to reprogram
straight away after it was re-soldered in place of the very first one. Third one was not re-soldered and allowed for some cycles
of reprogramming, but eventually also stopped to be erased.
Bad FRAM page address is 0x5800..0x6000. Cell values and page address remain the same for all the failed parts.
We excluded this page from the code mapping via corresponding linker directives so it works OK for the time being.
But we have some doubts remained regarding the nature of the effect and virtual possibility of it propagation to other
pages of memory during operation of a device.
The assembly of PCB-s was made at a plant using certified reflow soldering process.
To program the processors we use branded tools only.
Photo of the board you can find in the attachment.
Could you, please, give us some suggestions to the questions:
- What's the specificity of working with the MSP chips having FRAM as memory array?
- Are there some tricks and traps in using this memory as ordinary RAM with multiple access?
- Does it has limited value of erase/write cycles?
- Is there some errata for such an issue released?
- What is data retention period for this memory?
Thanks a lot.
Oleksandr
R&D engineer
Ukraine