Hi anyone...
i'm trying to implement ulp5.1 recommendation of moving my divide functions from flash into ram....
I've followed TI's example and the code does get put into ram as per the map file, but when viewed in the debugger dissassembly i see a whole lot of duplicated nonsense code (almost like default memory values) so naturally once the PC is set to the function it never returns!
MSP430F3736, CCS 6.1.2.00015, compiler tools 4.4.7, c/c++ dev tools 8.5.0.201409172108
MEMORY
{
SFR : origin = 0x0000, length = 0x0010
PERIPHERALS_8BIT : origin = 0x0010, length = 0x00F0
PERIPHERALS_16BIT : origin = 0x0100, length = 0x0100
RAM_EXECUTE : origin = 0x1C00, length = 0x0100
RAM : origin = 0x1D00, length = 0x1F00
INFOA : origin = 0x1980, length = 0x0080
INFOB : origin = 0x1900, length = 0x0080
INFOC : origin = 0x1880, length = 0x0080
INFOD : origin = 0x1800, length = 0x0080
FLASH_EXECUTE : origin = 0x4000, length = 0x0100 /
FLASH : origin = 0x4100, length = 0xBE80
FLASH2 : origin = 0x10000,length = 0x14000
INT00 : origin = 0xFF80, length = 0x0002
..etc
..etc
}
SECTIONS
{
.bss : {} > RAM /* Global & static vars */
.data : {} > RAM /* Global & static vars */
.TI.noinit : {} > RAM /* For #pragma noinit */
.sysmem : {} > RAM /* Dynamic memory allocation area */
.stack : {} > RAM (HIGH) /* Software system stack */
.run_from_ram : load = FLASH_EXECUTE, run = RAM_EXECUTE
#ifndef __LARGE_DATA_MODEL__
.text : {}>> FLASH /* Code */
#else
.text : {}>> FLASH2 | FLASH
..etc
..etc
}
#pragma CODE_SECTION(DivByInt32,".run_from_ram")
int32_t DivByInt32(int32_t valToDivide,int32_t divisor)
{
return(valToDivide/divisor);
}
#pragma CODE_SECTION(DivByInt16,".run_from_ram")
int32_t DivByInt16(int32_t valToDivide,int16_t divisor)
{
return(valToDivide/divisor);
}
thanks