This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am trying to use an EXP432P401R Launchpad to measure the current consumption of a custom MSP430F5528 board. I do not necessarily need to be debugging the MSP430 while measuring current, so I believe using the EXP432 launchpad in standalone EnergyTrace mode should be OK.
However, when I press the EnergyTrace button in the CCS Edit view the button remains pressed for ~10 seconds but nothing happens. Looking at the CCS log file I see the following exception:
!ENTRY org.eclipse.ui 4 0 2016-06-29 20:07:18.604 !MESSAGE Unhandled event loop exception !STACK 0 java.lang.IllegalArgumentException: No enum constant com.ti.dvt.energytrace.core.RuntimeParameter.EnumTargetDevice.RF432 at java.lang.Enum.valueOf(Enum.java:236) at com.ti.dvt.energytrace.core.RuntimeParameter$EnumTargetDevice.valueOf(RuntimeParameter.java:1) at com.ti.dvt.energytrace.af.PowerActivity$DebuggerTargetInfo.fromCCXML(PowerActivity.java:1198) at com.ti.dvt.energytrace.af.PowerActivity$DebuggerTargetInfo.<init>(PowerActivity.java:1166) at com.ti.dvt.energytrace.af.PowerActivity.launchHiddenDS(PowerActivity.java:1317) at com.ti.dvt.energytrace.IDEHandler.detectCfg(IDEHandler.java:290) at com.ti.dvt.energytrace.IDEHandler.launchHiddenDS(IDEHandler.java:376) at com.ti.dvt.energytrace.IDEHandler.preNonDebugStartup(IDEHandler.java:220) at com.ti.dvt.energytrace.IDEHandler.startupDashboard(IDEHandler.java:438) at com.ti.dvt.energytrace.actions.DashboardAction.runET(DashboardAction.java:102) at com.ti.dvt.energytrace.actions.DashboardAction.run(DashboardAction.java:55) at org.eclipse.ui.internal.PluginAction.runWithEvent(PluginAction.java:247) at org.eclipse.ui.internal.WWinPluginAction.runWithEvent(WWinPluginAction.java:228) at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:595) at org.eclipse.jface.action.ActionContributionItem.access$2(ActionContributionItem.java:511) at org.eclipse.jface.action.ActionContributionItem$6.handleEvent(ActionContributionItem.java:462) at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84) at org.eclipse.swt.widgets.Display.sendEvent(Display.java:4362) at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1113) at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180) at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3769) at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$4.run(PartRenderingEngine.java:1127) at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:337) at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1018) at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:156) at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:654) at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:337) at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:598) at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:150) at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:139) at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:380) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:235) at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method) at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:57) at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43) at java.lang.reflect.Method.invoke(Method.java:606) at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:669) at org.eclipse.equinox.launcher.Main.basicRun(Main.java:608) at org.eclipse.equinox.launcher.Main.run(Main.java:1515)
Also when I go to the EnergyTrace settings in CCS Preferences and press Apply/OK I get the following:
!ENTRY org.eclipse.jface 4 0 2016-06-29 19:59:07.603 !MESSAGE java.lang.NumberFormatException: empty String !STACK 0 java.lang.NumberFormatException: empty String at sun.misc.FloatingDecimal.readJavaFormatString(FloatingDecimal.java:1020) at java.lang.Double.valueOf(Double.java:504) at java.lang.Double.<init>(Double.java:597) at com.ti.dvt.energytrace.PreferencePage$DoubleFieldEditor.doStore(PreferencePage.java:223) at org.eclipse.jface.preference.FieldEditor.store(FieldEditor.java:683) at org.eclipse.jface.preference.FieldEditorPreferencePage.performOk(FieldEditorPreferencePage.java:344) at org.eclipse.jface.preference.PreferenceDialog$12.run(PreferenceDialog.java:925) at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:42) at org.eclipse.ui.internal.JFaceUtil$1.run(JFaceUtil.java:50) at org.eclipse.jface.util.SafeRunnable.run(SafeRunnable.java:173) at org.eclipse.jface.preference.PreferenceDialog.okPressed(PreferenceDialog.java:909) at org.eclipse.ui.internal.dialogs.FilteredPreferenceDialog.okPressed(FilteredPreferenceDialog.java:409) at org.eclipse.ui.internal.dialogs.WorkbenchPreferenceDialog.okPressed(WorkbenchPreferenceDialog.java:168) at org.eclipse.jface.preference.PreferenceDialog.buttonPressed(PreferenceDialog.java:233) at org.eclipse.jface.dialogs.Dialog$2.widgetSelected(Dialog.java:619) at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:248) at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84) at org.eclipse.swt.widgets.Display.sendEvent(Display.java:4362) at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1113) at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180) at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3769) at org.eclipse.jface.window.Window.runEventLoop(Window.java:827) at org.eclipse.jface.window.Window.open(Window.java:803) at org.eclipse.ui.internal.dialogs.WorkbenchPreferenceDialog.open(WorkbenchPreferenceDialog.java:211) at org.eclipse.ui.internal.OpenPreferencesAction.run(OpenPreferencesAction.java:63) at org.eclipse.jface.action.Action.runWithEvent(Action.java:473) at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:595) at org.eclipse.jface.action.ActionContributionItem.access$2(ActionContributionItem.java:511) at org.eclipse.jface.action.ActionContributionItem$5.handleEvent(ActionContributionItem.java:420) at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84) at org.eclipse.swt.widgets.Display.sendEvent(Display.java:4362) at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1113) at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180) at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3769) at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$4.run(PartRenderingEngine.java:1127) at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:337) at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1018) at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:156) at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:654) at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:337) at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:598) at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:150) at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:139) at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:380) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:235) at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method) at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:57) at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43) at java.lang.reflect.Method.invoke(Method.java:606) at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:669) at org.eclipse.equinox.launcher.Main.basicRun(Main.java:608) at org.eclipse.equinox.launcher.Main.run(Main.java:1515)
The only way to get the EnergyTrace window to even appear is to press the EnergyTrace button in while debugging a project, but even then pressing the start button has no effect, i.e. the button flashes to red for a sec then returns to green, time remains at 0sec and no data are plotted in the Energy or Power graphs.
I am using CCS 6.1.3 and have tested with the EXP432 both connected and not connected to USB and the target connection in EnergyTrace settings set to XDS110 and USB.
Shouldn't I be able to use the EXP432 in standalone EnergyTrace mode? Is there some other setting that I am missing?
Hi,
CCS should support standalone EnergyTrace with MSP432 LaunchPads.
But, you would first need to point EnergyTrace to launch using XDS110 by going to Windows --> Preferences --> Code Composer Studio --> Advanced Tools --> EnergyTrace Technology. And change the Target Connection from USB1 to XDS110.
Regards,
William
As I wrote in the first post I have already tried with both XDS110 and USB connection but get the errors described above.
Giannis Roussos said:The only way to get the EnergyTrace window to even appear is to press the EnergyTrace button in while debugging a project, but even then pressing the start button has no effect, i.e. the button flashes to red for a sec then returns to green, time remains at 0sec and no data are plotted in the Energy or Power graphs.
I've not seen the first problem you were facing with running EnergyTrace outside of a debug session, but I have had this problem while debugging. I think I get around it by pausing and running the target, which triggers EnergyTrace capture if the window is already open. After that the record button starts to work.
Hi Katie,
I tried (re)moving the EnergyTrace_RF432_XDS110.ccxml file but then EnergyTrace fails to start saying that no XDS110 is found.
Hi,
There are 2 similar files in the mentioned folder: "EnergyTrace_MSP432_XDS110.ccxml" and "EnergyTrace_RF432_XDS110.ccxml".
Please check that only the "RF432" one is removed and keep the "MSP432". Also make sure you have MSP432 Launchpad connected to your PC.
**Attention** This is a public forum