This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Quick question. Working with MSP430FR5736. Datasheet includes section on ADC10_B peripheral. And adc10_b files are there in driverlib includes. There is a working example for the 5739. Looking through, this I noticed a missing definition in the MSP430FR5736.h file (__MSP430_HAS_ADC10_B__) It's there in the MSP430FR5739.h ?!
Anyone able to confirm if the ADC10_B peripheral is actually there or not on the 5736? And if so, was it just fat fingers that the definition is missing in MSP430FR5736.h? Planning to build up a custom pcb, so would be great to confirm in advance.
Cheers,
Al.
**Attention** This is a public forum