Other Parts Discussed in Thread: ENERGIA
Dear sir,
I want to send the a characters from transmitter which is dynamically(means when i type character in serial monitor ),transmitter has to take that character and has to send to receiver at the other end.
so for this where should i change my code.I am doing code in energia.
/** * ---------------------------------------------------------------------------- * WirelessMonitorSensor.ino - wireless monitor sensor sketch using AIR430Boost ETSI driver. * Copyright (C) 2012-2013 Anaren Microwave, Inc. * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Lesser General Public * License as published by the Free Software Foundation; either * version 2.1 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Lesser General Public License for more details. * * You should have received a copy of the GNU Lesser General Public * License along with this library; if not, write to the Free Software * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA * * This example demonstrates usage of the AIR430BoostETSI library which uses * the 430Boost-CC110L AIR Module BoosterPack created by Anaren Microwave, Inc. * and available through the TI eStore, for the European Union. * * ---------------------------------------------------------------------------- * * Note: This file is part of AIR430Boost. * * ---------------------------------------------------------------------------- * * Description * =========== * * Acts as a simple transmitter for a star network. The sensor node can * transmit any type of message one-way using the broadcast address. To create * multiple networks, simply change the address on the hub node and have the * nodes in that network transmit to the assigned hub address. * * ---------------------------------------------------------------------------- * * This example assumes that two BoosterPacks will be used to showcase the * wireless radio communication functionality. This same code should be * programmed to both LaunchPad development kits. * * This BoosterPack relies on the SPI hardware peripheral and two additional * GPIO lines for SPI chip-select and GDO0 for packet handling. They use pins 18 * and 19 respectively. * * In the default configuration, this BoosterPack is not compatible with an * external crystal oscillator. This can be changed, if necessary, and would * require reconfiguration of the BoosterPack hardware and changes to the * AIR430BoostETSI library. Refer to the BoosterPack User's Manual if necessary. * * ETSI regulations must be followed when using this library. This example * limits the wireless duty cycle to 0.1% per ETSI. * * For complete information, please refer to the BoosterPack User's Manual * available at: * www.anaren.com/.../cc110l-air-module-boosterpack-embedded-antenna-module-anaren * * To purchase the 430Boost-CC110L AIR module BoosterPack kit, please visit the * TI eStore at: * estore.ti.com/430BOOST-CC110L-CC110L-RF-Module-BoosterPack-P2734.aspx */ /** * The AIR430BoostETSI library uses the SPI library internally. Energia does not * copy the library to the output folder unless it is referenced here. The order * of includes is also important due to this fact. */ #include <SPI.h> #include <AIR430BoostETSI.h> // ----------------------------------------------------------------------------- /** * Defines, enumerations, and structure definitions */ #define ADDRESS_LOCAL 0x02 #define ADDRESS_REMOTE 0x01 /** * sPacket - packet format. */ struct sPacket { uint8_t from; // Local node address that message originated from uint8_t message[59]; // Local node message [MAX. 59 bytes] }; // ----------------------------------------------------------------------------- /** * Global data */ struct sPacket txPacket; // ----------------------------------------------------------------------------- // Main example void setup() { // The radio library uses the SPI library internally, this call initializes // SPI/CSn and GDO0 lines. Also setup initial address, channel, and TX power. Radio.begin(ADDRESS_LOCAL, CHANNEL_1, POWER_MAX); txPacket.from = ADDRESS_LOCAL; memset(txPacket.message, 0, sizeof(txPacket.message)); // Setup serial for debug printing. Serial.begin(9600); /** * Setup LED for example demonstration purposes. * * Note: Set radio first to ensure that GDO2 line isn't being driven by the * MCU as it is an output from the radio. */ pinMode(RED_LED, OUTPUT); // Use red LED to display message reception digitalWrite(RED_LED, LOW); } void loop() { int i, j; delay(1000); // Send every second for (i = 0, j = '0'; i <= 0x2A; i++, j++) { txPacket.message[i] = j; } Radio.transmit(ADDRESS_REMOTE, (unsigned char*)&txPacket, sizeof(txPacket)); /** * Warning: ETSI regulations require duty cycling of 0.1% per hour. Changing * this may invalidate ETSI compliance. Some margin has been added. Please * refer to Anaren's A110LR09 User's Manual for more information. */ delay(500); }
/** * ---------------------------------------------------------------------------- * WirelessMonitorHub.ino - wireless monitor hub sketch using AIR430Boost ETSI driver. * Copyright (C) 2012-2013 Anaren Microwave, Inc. * * This library is free software; you can redistribute it and/or * modify it under the terms of the GNU Lesser General Public * License as published by the Free Software Foundation; either * version 2.1 of the License, or (at your option) any later version. * * This library is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * Lesser General Public License for more details. * * You should have received a copy of the GNU Lesser General Public * License along with this library; if not, write to the Free Software * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA * * This example demonstrates usage of the AIR430BoostETSI library which uses * the 430Boost-CC110L AIR Module BoosterPack created by Anaren Microwave, Inc. * and available through the TI eStore, for the European Union. * * ---------------------------------------------------------------------------- * * Note: This file is part of AIR430Boost. * * ---------------------------------------------------------------------------- * * Description * =========== * * Acts as a simple receiver for a star network. The hub node can receive both * broadcast messages and messages directed to its assigned address. The hub * node should not be assigned to address 0 (broadcast address). To create an * additional network, simply change the hub address. * * ---------------------------------------------------------------------------- * * This example assumes that two BoosterPacks will be used to showcase the * wireless radio communication functionality. This same code should be * programmed to both LaunchPad development kits. * * This BoosterPack relies on the SPI hardware peripheral and two additional * GPIO lines for SPI chip-select and GDO0 for packet handling. They use pins 18 * and 19 respectively. * * In the default configuration, this BoosterPack is not compatible with an * external crystal oscillator. This can be changed, if necessary, and would * require reconfiguration of the BoosterPack hardware and changes to the * AIR430BoostETSI library. Refer to the BoosterPack User's Manual if necessary. * * ETSI regulations must be followed when using this library. This example * limits the wireless duty cycle to 0.1% per ETSI. * * For complete information, please refer to the BoosterPack User's Manual * available at: * www.anaren.com/.../cc110l-air-module-boosterpack-embedded-antenna-module-anaren * * To purchase the 430Boost-CC110L AIR module BoosterPack kit, please visit the * TI eStore at: * estore.ti.com/430BOOST-CC110L-CC110L-RF-Module-BoosterPack-P2734.aspx */ /** * The AIR430BoostETSI library uses the SPI library internally. Energia does not * copy the library to the output folder unless it is referenced here. The order * of includes is also important due to this fact. */ #include <SPI.h> #include <AIR430BoostETSI.h> // ----------------------------------------------------------------------------- /** * Defines, enumerations, and structure definitions */ #define ADDRESS_LOCAL 0x01 /** * sPacket - packet format. */ struct sPacket { uint8_t from; // Local node address that message originated from uint8_t message[59]; // Local node message [MAX. 59 bytes] }; // ----------------------------------------------------------------------------- /** * Global data */ struct sPacket rxPacket; // ----------------------------------------------------------------------------- // Main example void setup() { // The radio library uses the SPI library internally, this call initializes // SPI/CSn and GDO0 lines. Also setup initial address, channel, and TX power. Radio.begin(ADDRESS_LOCAL, CHANNEL_1, POWER_MAX); rxPacket.from = 0; memset(rxPacket.message, 0, sizeof(rxPacket.message)); // Setup serial for debug printing. Serial.begin(9600); /** * Setup LED for example demonstration purposes. * * Note: Set radio first to ensure that GDO2 line isn't being driven by the * MCU as it is an output from the radio. */ pinMode(RED_LED, OUTPUT); // Use red LED to display message reception digitalWrite(RED_LED, LOW); } void loop() { // Turn on the receiver and listen for incoming data. Timeout after 1 seconds. // The receiverOn() method returns the number of bytes copied to rxData. if (Radio.receiverOn((unsigned char*)&rxPacket, sizeof(rxPacket), 1000) > 0) { digitalWrite(RED_LED, HIGH); Serial.print("FROM: "); Serial.print(rxPacket.from); Serial.print(" MSG: "); Serial.println((char*)rxPacket.message); digitalWrite(RED_LED, LOW); } // Note: This sketch never transmits so no additional delay required to meet ETSI // requirements. }
these are my transmitter and receiver code...........please let me knw where i have to change the code.
thank you