This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Guys,
I am a little bit confused here. As I need PORT3 PIN0 as a chip select port for SPI I defined HIGH and LOW macros with the appropriate driver lib functions. As I was debugging my program, I wondered why the chip select doesn't go high, even if the register value is 1. So I started to measure, but the PIN actually isn't on Vcc.
How is this possible..even if the register value tells the opposite.
I am unfortunetely using an XMS-chip version on a custom board.
best regards
Benni
**Attention** This is a public forum