This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to modify uCOS-III source codes when MSP432's FPU is enabled?



Hi, I'm working on a project with MSP432P401R launchpad.  And I have already ported uCOS-III v3.05 to it successfully.

But when I add some functions which deal with float point data, the uCOS-III runs into App_Fault_ISR().

As far as I know,   FPU of MSP432 is enabled in default when compiled under CCS Studio v6.1.3.

While uCOS-III does not support FPU feature defaultly, so I have modified *OSTaskStkInit

CPU_STK  *OSTaskStkInit (OS_TASK_PTR    p_task,
                         void          *p_arg,
                         CPU_STK       *p_stk_base,
                         CPU_STK       *p_stk_limit,
                         CPU_STK_SIZE   stk_size,
                         OS_OPT         opt)
{
    CPU_STK    *p_stk;

    
    (void)opt;                                                  /* Prevent compiler warning                               */

    p_stk = &p_stk_base[stk_size];                              /* Load stack pointer                                     */
                                                                /* Align the stack to 8-bytes.                            */
    p_stk = (CPU_STK *)((CPU_STK)(p_stk) & 0xFFFFFFF8);
                                                                /* Registers stacked as if auto-saved on exception        */
#if(OS_CPU_ARM_FP_EN == DEF_ENABLED)
    *--p_stk = (CPU_STK)0x00000000u;                            /* No Name Register                                       */
    *--p_stk = (CPU_STK)0x00000000u;                            /* FPSCR                                                  */
    *--p_stk = (CPU_STK)0x15151515u;                            /* S15                                                    */
    *--p_stk = (CPU_STK)0x14141414u;                            /* S14                                                    */
    *--p_stk = (CPU_STK)0x13131313u;                            /* S13                                                    */
    *--p_stk = (CPU_STK)0x12121212u;                            /* S12                                                    */
    *--p_stk = (CPU_STK)0x11111111u;                            /* S11                                                    */
    *--p_stk = (CPU_STK)0x10101010u;                            /* S10                                                    */
    *--p_stk = (CPU_STK)0x09090909u;                            /* S9                                                     */
    *--p_stk = (CPU_STK)0x08080808u;                            /* S8                                                     */
    *--p_stk = (CPU_STK)0x07070707u;                            /* S7                                                     */
    *--p_stk = (CPU_STK)0x06060606u;                            /* S6                                                     */
    *--p_stk = (CPU_STK)0x05050505u;                            /* S5                                                     */
    *--p_stk = (CPU_STK)0x04040404u;                            /* S4                                                     */
    *--p_stk = (CPU_STK)0x03030303u;                            /* S3                                                     */
    *--p_stk = (CPU_STK)0x02020202u;                            /* S2                                                     */
    *--p_stk = (CPU_STK)0x01010101u;                            /* S1                                                     */
    *--p_stk = (CPU_STK)0x00000000u;                            /* S0                                                     */
#endif
    *--p_stk = (CPU_STK)0x01000000u;                            /* xPSR                                                   */
    *--p_stk = (CPU_STK)p_task;                                 /* Entry Point                                            */
    *--p_stk = (CPU_STK)OS_TaskReturn;                          /* R14 (LR)                                               */
    *--p_stk = (CPU_STK)0x12121212u;                            /* R12                                                    */
    *--p_stk = (CPU_STK)0x03030303u;                            /* R3                                                     */
    *--p_stk = (CPU_STK)0x02020202u;                            /* R2                                                     */
    *--p_stk = (CPU_STK)p_stk_limit;                            /* R1                                                     */
    *--p_stk = (CPU_STK)p_arg;                                  /* R0 : argument                                          */
                                                                /* Remaining registers saved on process stack             */
#if (OS_CPU_ARM_FP_EN == DEF_ENABLED)
    *--p_stk = (CPU_STK)0x31313131u;                            /* S31                                                    */
    *--p_stk = (CPU_STK)0x30303030u;                            /* S30                                                    */
    *--p_stk = (CPU_STK)0x29292929u;                            /* S29                                                    */
    *--p_stk = (CPU_STK)0x28282828u;                            /* S28                                                    */
    *--p_stk = (CPU_STK)0x27272727u;                            /* S27                                                    */
    *--p_stk = (CPU_STK)0x26262626u;                            /* S26                                                    */
    *--p_stk = (CPU_STK)0x25252525u;                            /* S25                                                     */
    *--p_stk = (CPU_STK)0x24242424u;                            /* S24                                                     */
    *--p_stk = (CPU_STK)0x23232323u;                            /* S23                                                     */
    *--p_stk = (CPU_STK)0x22222222u;                            /* S22                                                     */
    *--p_stk = (CPU_STK)0x21212121u;                            /* S21                                                     */
    *--p_stk = (CPU_STK)0x20202020u;                            /* S20                                                     */
    *--p_stk = (CPU_STK)0x19191919u;                            /* S19                                                     */
    *--p_stk = (CPU_STK)0x18181818u;                            /* S18                                                     */
    *--p_stk = (CPU_STK)0x17171717u;                            /* S17                                                     */
    *--p_stk = (CPU_STK)0x16161616u;                            /* S16                                                     */
#endif
    *--p_stk = (CPU_STK)0x11111111u;                            /* R11                                                    */
    *--p_stk = (CPU_STK)0x10101010u;                            /* R10                                                    */
    *--p_stk = (CPU_STK)0x09090909u;                            /* R9                                                     */
    *--p_stk = (CPU_STK)0x08080808u;                            /* R8                                                     */
    *--p_stk = (CPU_STK)0x07070707u;                            /* R7                                                     */
    *--p_stk = (CPU_STK)0x06060606u;                            /* R6                                                     */
    *--p_stk = (CPU_STK)0x05050505u;                            /* R5                                                     */
    *--p_stk = (CPU_STK)0x04040404u;                            /* R4                                                     */

    return (p_stk);
}

and the OS_CPU_PendSVHandler() function

    .asmfunc
OS_CPU_PendSVHandler:
    CPSID   I                                                   ; Prevent interruption during context switch
    MRS     R0, PSP                                             ; PSP is process stack pointer
;.if __TI_TMS470_V7M4__ & __TI_VFP_SUPPORT__
    VSTMDB    R0!, {S16-S31}                                 ; Save remaining regs s31-s16 on stack
;.endif
    STMFD   R0!, {R4-R11}                                       ; Save remaining regs r4-11 on process stack

    LDR     R5, OSTCBCurPtrAddr                                 ; OSTCBCurPtr->OSTCBStkPtr = SP;
    LDR     R6, [R5]
    STR     R0, [R6]                                            ; R0 is SP of process being switched out

                                                                ; At this point, entire context of process has been saved
    MOV     R4, LR                                              ; Save LR exc_return value
    BL      OSTaskSwHook                                        ; OSTaskSwHook();

    LDR     R0, OSPrioCurAddr                                   ; OSPrioCur   = OSPrioHighRdy;
    LDR     R1, OSPrioHighRdyAddr
    LDRB    R2, [R1]
    STRB    R2, [R0]

    LDR     R1, OSTCBHighRdyPtrAddr                             ; OSTCBCurPtr = OSTCBHighRdyPtr;
    LDR     R2, [R1]
    STR     R2, [R5]


    ORR     LR, R4, #0xF4                                       ; Ensure exception return uses process stack
    LDR     R0, [R2]                                            ; R0 is new process SP; SP = OSTCBHighRdyPtr->StkPtr;
    LDMFD   R0!, {R4-R11}                                       ; Restore r4-11 from new process stack
    .if __TI_TMS470_V7M4__ & __TI_VFP_SUPPORT__
    VLDMIA   R0!, {S16-S31}
    .endif
    MSR     PSP, R0                                             ; Load PSP with new process SP
    CPSIE   I
    BX      LR                                                  ; Exception return will restore remaining context
    .endasmfunc

.end

In addition, I add "__VFP_FP__" predefine in project config.

Also the "OS_OPT_TASK_SAVE_FP" option is enabled when task in uCOS-III is created.

Despire all the changes, the uCOS-III still runs into App_Fault_ISR() routine after the first task is switch out.

Any one has any idea about the issue? Thank you vech much!

 

  • The FPU is not enabled after reset.

    www.ti.com/lit/pdf/slau356

    Page 81
    www.ti.com/.../slau356d.pdf

    In the CCS settings the variable is _FPU_USED is defined and in the system_msp432p401r.c the FPU is enabled.

    void SystemInit(void)
    {
    // Enable FPU if used
    #if (__FPU_USED == 1) /* __FPU_USED is defined in core_cm4.h */
    SCB->CPACR |= ((3UL << 10 * 2) | /* Set CP10 Full Access */
    (3UL << 11 * 2)); /* Set CP11 Full Access */
    #endif

    I hope this provides some insight.

    Regards,
    Chris
  • Chris Sterzik said:
    The FPU is not enabled after reset.

    www.ti.com/lit/pdf/slau356

    Page 81
    www.ti.com/.../slau356d.pdf

    In the CCS settings the variable is _FPU_USED is defined and in the system_msp432p401r.c the FPU is enabled.

    void SystemInit(void)
    {
    // Enable FPU if used
    #if (__FPU_USED == 1) /* __FPU_USED is defined in core_cm4.h */
    SCB->CPACR |= ((3UL << 10 * 2) | /* Set CP10 Full Access */
    (3UL << 11 * 2)); /* Set CP11 Full Access */
    #endif

    I hope this provides some insight.

    Regards,
    Chris

    Thank you for your reply first, but the fact is not like what you said above.

    Under uCOS-3, when power on, system runs into App_Reset_ISR(), then it will run into " _c_int00" assembly routine. Just at the head of " _c_int00" in file "boot.asm", there are instructions as below.

    _c_int00: .asmfunc stack_usage(0)

        .if !__TI_ARM_V7M__ & !__TI_ARM_V6M0__
        .if __TI_NEON_SUPPORT__ | __TI_VFP_SUPPORT__
          .................................
            .else ; !__TI_ARM_V7M & !__TI_ARM_V6M0
        .if __TI_TMS470_V7M4__ & __TI_VFP_SUPPORT__
        .thumb
        ;*------------------------------------------------------
        ;* SETUP FULL ACCESS TO COPROCESSORS 10 AND 11,
        ;* REQUIRED FOR FP. COPROCESSOR ACCESS CONTROL REG
        ;* BITS [23:22] - CP11, [21:20] - CP10
        ;* SET TO 0b11 TO ENABLE FULL ACCESS
            ;*------------------------------------------------------
    cpacr   .set     0xE000ED88            ; CAPCR address
        MOVW     r1, #cpacr & 0xFFFF
        MOVT     r1, #cpacr >> 16
        LDR      r0, [ r1 ]
               MOV      r3, #0xf0
        ORR      r0,r0,r3, LSL #16
        STR      r0, [ r1 ]
        ;*---------added by Charles Chen------------------------
        ;*---------reset pipeline ------------------------------
        ;*---------according to MSP432P4xx.pdf------------------
        ;DSB
        ISB
        .thumb
        .endif ; __TI_TMS470_V7M4__ & __TI_VFP_SUPPORT__
        .endif ; !__TI_ARM_V7M & !__TI_ARM_V6M0__

    These are the very codes that enable FPU of MSP432. So no need to re-enable FPU in C file.

    While good news is that I have found the cause of the issue I posted. It is related with uCOS-3 v3.05 source files about FPU register stacking handling.

    Thank you still the same.

**Attention** This is a public forum