This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432 Launchpad - CS_DAP_0: Error connecting to the target: (Error -260 @ 0x0)

Hi,

I am unable to connect to the MSP432 Launchpad. I have browsed through the forums and tried the following potential solutions:

1. Factory reset -  same error occurs when I right click-> connect target on the device under non-debuggable devices after rightclick->show all cores.

2. Changing JTAG/SWD mode - I tried all the modes that are present in the drop down menu and factory reset did not work with any of them.

3. Another thread reply asked to remove all JTAG connectors on J101 and check to see if XDS100 shows up in Device Manager in Windows. And connect each one back until it disappears again - XDS100 doesn't show up in any combination, all jumpers connected to none.

And another thing I would like to mention is that I had the same error with another board - one of the black ones with a switch for External Debug/XDS ET. It just happened that the switch was in the wrong place and flicking it back in place solved the issue. I was able to factory reset and that board is fine now.

But the board I have this problem now with is one of the red ones and I can't find this switch on it anywhere.

And I think my error might have come from changing the startup file (startup_msp432p401r_ccs.c) because this error occurred after I dumped that particular project onto the board. Please find the project attached and check if you can reproduce the error.

Thanks!

empty_project.zip

  • Hello,
    Thank you for searching through the forum and exercising some of the fixes previously discussed. You mentioned that you have had some success with the black launch pads (revision B silicon) but not the red launch pads (revision C). Have you done the updates recommended in this thread?

    e2e.ti.com/.../540690

    If you have removed all of the jumpers from J101 and are still not able to even see the XDS in the device manager, then I am not certain the migration will help. You may want to test on another machine or another USB port.

    Chris

**Attention** This is a public forum