This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Missing GPIO pins in the MSP432p401R Launchpad for SPI communication

Part Number: MSP432P401R

Fellow MSP users,

I tried implementing a SPI communicaion with a SD card using the above MCU but found unable to do it since a required pin for clock output was missing in the 3rd port (P3.1).

So I tried moving to Port 2, but found the P2.1  (UCAxCLK) pin missing again. I looked into some graphical maps of the pin configuration and found that the SCK pin was given in the P5.1 pin,

but the Port 5 doesn't provide with SPI compatibility according to Technical Guide (slau356) and User Guide (slau597b). Why are some pins missing? How can I solve this problem (that is finding a pin to get

the clock output pin)?

Graphical pin configuration

energia.nu/.../2016-06-09-LaunchPads-MSP432-2.0-—-Pins-Maps.jpg

The programming was done at register level due to driverlib.h malfunctioning so I have a general idea about the SPI and Clock System in MSP432 .

I haven't completed the code yet.

Please can some person with an expirienced knowledge help me with the issue.

(This is my first time using a MSP MCU).

Best regards,

Inoth Munisinghe.

**Attention** This is a public forum