This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hi,
I'm using custom board with MCU as MSP432P401R.
I'm trying to communicate msp432 as a master and enc424j600(ethernet) as a slave with spi connection.
I found out that when spi receiver(MISO) interrupt occurs clk(P1.5) doesn't give any signal.
However when transmitting data(MOSI) I can see clk signal with oscilloscope.
Is there any solution or suggestion why spi reciever or clk don't work?
Here comes the code!!
/*
*
* MSP432 = SPI master, external device = SPI slave
*
* MSP432P401R
* -----------------
* | |
* | P1.4 |-> CS
* | |
* | P1.6 |-> Data Out (UCB0SIMO)
* | |
* | P1.7 |<- Data In (UCB0SOMI)
* | |
* | P1.5 |-> Serial Clock Out (UCB0CLK)
*******************************************************************************/
const eUSCI_SPI_MasterConfig spiMasterConfig =
{
EUSCI_B_SPI_CLOCKSOURCE_SMCLK, // SMCLK Clock Source
24000000,
500000,
EUSCI_B_SPI_MSB_FIRST,
EUSCI_B_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT,
EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH,
EUSCI_B_SPI_3PIN
};
int main(void)
{
int Result;
uint16_t Result1;
BTPS_Initialization_t BTPS_Initialization;
HCI_DriverInformation_t HCI_DriverInformation;
HCI_HCILLConfiguration_t HCILLConfig;
HCI_Driver_Reconfigure_Data_t DriverReconfigureData;
/* Configure the hardware for its intended use. */
HAL_ConfigureHardware();
/* Flag that sleep is not currently enabled. */
SleepAllowed = FALSE;
/* Configure the UART Parameters. */
HCI_DRIVER_SET_COMM_INFORMATION(&HCI_DriverInformation, 1, HAL_HCI_UART_MAX_BAUD_RATE, cpHCILL_RTS_CTS);
HCI_DriverInformation.DriverInformation.COMMDriverInformation.InitializationDelay = 100;
/* Set up the application callbacks. */
BTPS_Initialization.GetTickCountCallback = HAL_GetTickCount;
BTPS_Initialization.MessageOutputCallback = HAL_ConsoleWrite;
/* Initialize the application. */
if((Result = InitializeApplication(&HCI_DriverInformation, &BTPS_Initialization)) > 0)
{
/* Save the Bluetooth Stack ID. */
BluetoothStackID = (unsigned int)Result;
BTPS_Delay(200);
GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN4);
GPIO_setAsPeripheralModuleFunctionInputPin (GPIO_PORT_P1, GPIO_PIN7 | GPIO_PIN6 | GPIO_PIN5 , GPIO_PRIMARY_MODULE_FUNCTION);
GPIO_setAsOutputPin(GPIO_PORT_P1,GPIO_PIN4);
GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN4);
MAP_SPI_initMaster(EUSCI_B0_BASE, &spiMasterConfig);
MAP_SPI_enableModule(EUSCI_B0_BASE);
MAP_SPI_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_SPI_RECEIVE_INTERRUPT);
Interrupt_enableInterrupt(INT_EUSCIB0);
MAP_Interrupt_disableInterrupt(INT_EUSCIB0);
MAP_Interrupt_disableInterrupt(INT_EUSCIB0);
BTPS_Delay(100);
GPIO_setOutputLowOnPin(GPIO_PORT_P1,GPIO_PIN4);
//while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
MAP_SPI_transmitData(EUSCI_B0_BASE, 0x22);
//while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
MAP_SPI_transmitData(EUSCI_B0_BASE, 0x16);
//while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
MAP_SPI_transmitData(EUSCI_B0_BASE, 0x33);
//while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
MAP_SPI_transmitData(EUSCI_B0_BASE, 0x31);
GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN4);
BTPS_Delay(1);
GPIO_setOutputLowOnPin(GPIO_PORT_P1,GPIO_PIN4);
//while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
MAP_SPI_transmitData(EUSCI_B0_BASE, 0x20);
//while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
MAP_SPI_transmitData(EUSCI_B0_BASE, 0x16);
BTPS_Delay(1);
while (MAP_GPIO_getInputPinValue(GPIO_PORT_P1, GPIO_PIN7));
Interrupt_enableInterrupt(INT_EUSCIB0);
GPIO_setOutputHighOnPin(GPIO_PORT_P1,GPIO_PIN4);
Display(("%d \r\n",a));
/* We need to execute Add a function to process the command line */
/* to the BTPS Scheduler. */
if(BTPS_AddFunctionToScheduler(ProcessCharactersTask, NULL, 100))
{
/* Add the idle task (which determines if LPM3 may be entered) */
/* to the scheduler. */
if(BTPS_AddFunctionToScheduler(IdleTask, NULL, 100))
{
if(BTPS_AddFunctionToScheduler(ToggleLEDTask, NULL, 750))
{
HAL_SetLEDColor(hlcGreen);
/* Execute the scheduler, note that this function does */
/* not return. */
BTPS_ExecuteScheduler();
}
}
}
}
/* If we've gotten to this point then an error has occurred, set the */
/* LED to red to signify that there is a problem. */
HAL_SetLEDColor(hlcRed);
/* Poll the error flags to see if we can determine the reason for the*/
/* failure. */
PollErrorFlags();
/* Scheduler above should run continuously, if it exits an error */
/* occurred. */
while(1)
{
HAL_ToggleLED();
BTPS_Delay(100);
}
}
void EUSCIB0_IRQHandler(void)
{
//GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN4);
uint32_t status = SPI_getEnabledInterruptStatus(EUSCI_B0_BASE);
SPI_clearInterruptFlag(EUSCI_B0_BASE, status);
if(status & EUSCI_B_SPI_RECEIVE_INTERRUPT)
{
/* USCI_B0 TX buffer ready? */
while (!(SPI_getInterruptStatus(EUSCI_B0_BASE, EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
RXData = MAP_SPI_receiveData(EUSCI_B0_BASE);
Display(("RXData = %x\r\n",RXData));
//BTPS_Delay(10);
//GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN4);
}
}
Hello,
Because you are the master, you will need to provide the clock so the slave can send its data. For example, the following function transmits a dummy 0xFF and then it reads the RX buffer
int spi_Read(unsigned char *pBuff, int len) { int i = 0; ASSERT_CS(); for (i = 0; i < len; i ++) { while (!(UCB0IFG&UCTXIFG)); UCB0TXBUF = 0xFF; while (!(UCB0IFG&UCRXIFG)); pBuff[i] = UCB0RXBUF; } DEASSERT_CS(); return len; }
Hopefully this helps.
David
**Attention** This is a public forum