Part Number: MSP430FR2532
Other Parts Discussed in Thread: MSP430FR2632
Hello.
I have three questions.
1.Is it possible to realize sliders using MSP430RE2532?
2.Are there any APIs or guidelines to transmit capTIivate sensing data from MSP430FR2532 to Host MPU via serial interface?
I want to control capTIvate touch sensor in MSP430FR2532 by host MCU or MPU via SPI / I2C / UART.
But I think that development is difficult without APIs or guidelines.
3.Is it possible to realize slider "Metal Touch Solution" with 2mm x 20mm layout?
If you don't know about this question or the answer is "NO",I'm happy to give you some anticipated concerns.
If answer of question 1 is "No".
Question 2 and 3 answers can be referred to other CapTIvate devices.
Could you give me something advises?
Regards,
uchida-k