This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Hi! I am a student working on my senior capstone project at UT Austin, and our team is trying to use the MSP432P401RIPZR chip for a custom PCB design. I was looking at the hardware resources and the BOM, and tried to find the high frequency 48 MHz crystal that is used on the LaunchPad, but the product from DigiKey can only be purchased in bulk (1000+).
DigiKey offered the following alternative (linked). It looks like it should be more stable, same load capacitance, but the ESR is 50 Ohms, instead of 40 Ohms. I know the crystal and capacitors surrounding it are a delicate system; do y'all think that this alternative will work?
Hmm, thanks for the info! Didn't see that in the datasheet before.
I still don't know what crystal to use, though. :( I can't seem to find anything on DigiKey, Mouser, Newark, Arrow, etc. that fits the specs. It's hard enough to find a 40 Ohm ESR part; I can't find any 30 or 15 Ohm crystals.
If anyone knows of any stock crystals that should work, I would greatly appreciate it! :)
Jiacheng Jason He said:I still don't know what crystal to use, though. :( I can't seem to find anything on DigiKey, Mouser, Newark, Arrow, etc. that fits the specs. It's hard enough to find a 40 Ohm ESR part; I can't find any 30 or 15 Ohm crystals.
Are you going to design mass-product for industrial temperature range? If not - then you can relax requirements, especially if you plan to build prototype first.
**Attention** This is a public forum