This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Hi,
I want to know if I can power the board using 5 V connector (J7) or only using J6 jump with 3.3. User guide says you have to use J6 with 3.3V but I read a forum post speaking about the use the J7 pin with 5V
MSP432P401R External Battery - MSP low-power microcontroller forum - MSP low-power microcontrollers ...
Best regards,
**Attention** This is a public forum