This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: MSP432P401R Launchpad - External power

Part Number: MSP432P401R

Hi,

I want to know if I can power the board using 5 V connector (J7) or only using J6 jump with 3.3. User guide says you have to use J6 with 3.3V but I read a forum post speaking about the use the J7 pin with 5V

MSP432P401R External Battery - MSP low-power microcontroller forum - MSP low-power microcontrollers ...

e2e.ti.com
I tried to connect 3.3V External Battery to the MSP432P401R Launchpad to the Pins (3.3v / Gnd) on the Right of the board - it did not work. However, when I connected

Best regards,

**Attention** This is a public forum