This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
I would like to know how to connect an external 5V power supply (not via the USB port) to power up my MSP432 P401R (Red) launchpad.
What jack to use and any jumpers to insert/remove?
Thanks
Hello,
Please keep in mind that the MSP432P4 voltage range goes from 1.62 to 3.7V. Having said that, you will need to use Launchpad regulator, therefore:
1. Use the 5V Header (J7) to connect the 5V external power supply.
2. Remove all the jumpers from J101 except GND, 3V3 and 5V.
I'm assuming that you will be using and external debugger but I just want to make sure that is the case.
Hopefully this helps.
David
Can i leave the RST jumper on, in order to still use the MSP432 reset switch S3 to reset the MSP432 processor if needed ?
Thanks
**Attention** This is a public forum