This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401M: In MSP432 could I configure I2C interface to Master while using in bootloader via P3.6 - P3.7

Part Number: MSP432P401M


Hi All,

Could anyone explain me next moment:

In my system I would like to use FT200XD device (USB - I2C slave IC). It is a slave, so MSP432 configured to be the I2C master.

FT200XD connected via  P3.6 - P3.7.

Could this configuration be used for bootloading purposes or I need to change the device FT200XD to (I2C master)?

If it is a possible configuration what should be done?

Explained answers are welcomed.

Kind regards,

Andrei Zinenko

**Attention** This is a public forum