Part Number: MSP430F6779
Hi, all
I have a question about MSP430 Errata of SD24_B Module.
1)Is this errata applied only in case of -VFS MAX voltage ,or from zero to -VFS MAX range at the input?
2)Does an erroneous output mean fixed value or indefinite value?
The SD3 of MSP430F6779 Device Errata described as below:
Function:
Incorrect conversion result in twos complement mode when -VFS is applied
Description:
When the SD converter is configured in twos complement mode with left or right
alignment and any OSR setting, applying the -VFS voltage at the input will result in an
erroneous output.
best regards,
kyt