Tool/software: Code Composer Studio
Hello,
I'm having difficulty configuring the ADXL345 accelerometer with the MSP430FR5969 Launchpad.
I've been following along with a similar solution posted here. I believe the hook-up is identical:
GND -> GND
VCC -> VCC
CS -> VCC
SDO -> GND
SDA -> P1.7 (with 4.7k pullup resistor)
SCL -> P1.6 (with 4.7k pullup resistor)
My buffer never seems to fill after running Debug. So I imagine I'm initializing something incorrectly.
One of my peers mentioned that I may need to add a clock initialization procedure?
I've tested the ADXL345 on an Arduino and it works fine, so I don't believe it's a hardware problem.
Any advice it welcomed, thank you.
I've attached my modification of the code here:
#include <msp430.h> #define NUM_BYTES_TX 2 #define NUM_BYTES_RX 6 #define ADXL_345 0x53 int RXByteCtr, x, y, z; volatile unsigned char RxBuffer[6]; // Allocate 6 byte of RAM unsigned char *PRxData; // Pointer to RX data unsigned char TXByteCtr, RX = 0; unsigned char MSData[2]; // Functions for I2C void Setup_TX(unsigned char); void Setup_RX(unsigned char); void Transmit(unsigned char,unsigned char); void TransmitOne(unsigned char); void Receive(void); int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop WDT // LED P1OUT &= ~BIT0; // Clear P1.0 output latch P1DIR |= BIT0; // P1.0 = red LED P1OUT |= BIT0; // P1.0 = red LED P1SEL1 |= BIT6 + BIT7; // I2C pins // Disable the GPIO power-on default high-impedance mode to activate // previously configured port settings PM5CTL0 &= ~LOCKLPM5; // Init sequence for ADXL345 Setup_TX(ADXL_345); Transmit(0x2D,0x00); while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent Setup_TX(ADXL_345); Transmit(0x2D,0x10); while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent Setup_TX(ADXL_345); Transmit(0x2D,0x08); while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent while(1){ // Transmit process Setup_TX(ADXL_345); TransmitOne(0x32); // Request Data from ADXL345 in 2g Range 10Bit resolution while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent // Receive process Setup_RX(ADXL_345); Receive(); while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent x = (((int)RxBuffer[1]) << 8) | RxBuffer[0]; y = (((int)RxBuffer[3]) << 8) | RxBuffer[2]; z = (((int)RxBuffer[5]) << 8) | RxBuffer[4]; // Now we have x,y,z reading. // Below red LED is on, if x or y angle is more then 45 or less then -45 degree. if ((x > 128) || (y > 128) || (x < -128) || (y < -128)) { P1OUT |= BIT0; // red LED on } else { P1OUT &= ~BIT0; // red LED off } __delay_cycles(1000000); // delay 1 sec } } //------------------------------------------------------------------------------- // I2C //------------------------------------------------------------------------------- #pragma vector = USCI_B0_VECTOR __interrupt void USCI_B0_ISR(void) { if(RX == 1){ // Master Recieve? RXByteCtr--; // Decrement RX byte counter if (RXByteCtr) { *PRxData++ = UCB0RXBUF; // Move RX data to address PRxData } else { UCB0CTLW1 |= UCTXSTP; // No Repeated Start: stop condition *PRxData++ = UCB0RXBUF; // Move final RX data to PRxData __bic_SR_register_on_exit(LPM0_bits | GIE); // Exit LPM0 }} else{ // Master Transmit if (TXByteCtr) // Check TX byte counter { TXByteCtr--; // Decrement TX byte counter UCB0TXBUF = MSData[TXByteCtr]; // Load TX buffer } else { UCB0CTLW1 |= UCTXSTP; // I2C stop condition UCB0IFG &= ~UCTXIFG; // Clear USCI_B0 TX int flag __bic_SR_register_on_exit(LPM0_bits | GIE); // Exit LPM0 } } } void Setup_TX(unsigned char Dev_ID){ _DINT(); RX = 0; UCB0IE &= ~UCRXIE; // Disable USCI_B0 RX interrupt while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent// Disable RX interrupt UCB0CTLW1 |= UCSWRST; // Enable SW reset UCB0CTLW0 = UCMODE_3 | UCMST | UCSYNC; // I2C Master, synchronous mode UCB0CTLW1 = UCSSEL_2; // Use SMCLK, keep SW reset UCB0BR0 = 0x0008; // baudrate = SMCLK / 8 UCB0TBCNT = 0x0006; // number of bytes to be received UCB0I2CSA = Dev_ID; // Slave Address is 048h UCB0CTLW1 &= ~UCSWRST; // Clear SW reset, resume operation UCB0IE |= UCTXIE | UCNACKIE | UCBCNTIE; // Enable TX interrupt } void Setup_RX(unsigned char Dev_ID){ _DINT(); RX = 1; UCB0IE &= ~UCRXIE; // Disable USCI_B0 RX interrupt UCB0CTLW1 |= UCSWRST; // Enable SW reset UCB0CTLW0 = UCMODE_3 | UCMST | UCSYNC; // I2C Master, synchronous mode UCB0CTLW1 = UCSSEL_2; // Use SMCLK, keep SW reset UCB0BR0 = 0x0008; // baudrate = SMCLK / 8 UCB0TBCNT = 0x0006; UCB0I2CSA = Dev_ID; // Slave Address is 048h UCB0CTLW1 &= ~UCSWRST; // Clear SW reset, resume operation UCB0IE |= UCRXIE | UCNACKIE | UCBCNTIE; // Enable RX interrupt } void Transmit(unsigned char Reg_ADD,unsigned char Reg_DAT){ MSData[1]= Reg_ADD; MSData[0]= Reg_DAT; TXByteCtr = NUM_BYTES_TX; // Load TX byte counter while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition while (1) { __delay_cycles(2000); while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent UCB0CTLW1 |= UCTXSTT; // I2C start condition } } void TransmitOne(unsigned char Reg_ADD){ MSData[0]= Reg_ADD; TXByteCtr = 1; // Load TX byte counter while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent UCB0CTLW1 |= UCTR + UCTXSTT; // I2C TX, start condition while (1) { __delay_cycles(2000); while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent UCB0CTLW1 |= UCTXSTT; // I2C start condition } } void Receive(void){ PRxData = (unsigned char *)RxBuffer; // Start of RX buffer RXByteCtr = NUM_BYTES_RX; // Load RX byte counter while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent UCB0CTLW1 |= UCTXSTT; // I2C start condition while (1) { __delay_cycles(2000); while (UCB0CTLW1 & UCTXSTP); // Ensure stop condition got sent UCB0CTLW1 |= UCTXSTT; // I2C start condition } }