Part Number: MSP430F5419A
Tool/software: Code Composer Studio
My code size just reached the point where I need to use the large memory model.
I am using GCC GNU v5.3.0.219. on Code Composer Studio Version: 6.2.0.00050 (Linux)
Are there any examples or tutorials on how to switch to the large memory model with the GCC tools?
I added -mlarge flag to the compiler and linker.
I am still getting:
/opt/ti-6.2.0/ccsv6/tools/compiler/gcc_msp430_5.3.0.219/bin/../lib/gcc/msp430-elf/5.3.0/../../../../msp430-elf/bin/ld: xxxx.out section `.text' will not fit in region `ROM'
/opt/ti-6.2.0/ccsv6/tools/compiler/gcc_msp430_5.3.0.219/bin/../lib/gcc/msp430-elf/5.3.0/../../../../msp430-elf/bin/ld: section __interrupt_vector_45 loaded at [0000ffd8,0000ffd9] overlaps section .text loaded at [00007008,00011f5b]
/opt/ti-6.2.0/ccsv6/tools/compiler/gcc_msp430_5.3.0.219/bin/../lib/gcc/msp430-elf/5.3.0/../../../../msp430-elf/bin/ld: region `ROM' overflowed by 8156 bytes
Also, what is the correct way to configure hardware registers such as DMAxDA and DMAxSA that hold addresses?
I tried:
char myBuffer[10];
__data16_write_addr((unsigned short) &DMA1SA, (unsigned long) myBuffer);
and I am getting
warning: cast from pointer to integer of different size [-Wpointer-to-int-cast]
Thanks