Part Number: MSP430F5419A
Other Parts Discussed in Thread: MSP-FET, , UNIFLASH
Sometimes this works and other times I get the ERROR 59. My computer is Windows 7. Using an MSP-FET tool.
This is what I'm running at the command prompt:
c:\ti\mspflasher_1.3.20\msp430flasher.exe -i COM10 -n "msp430F5419a" -w "c:\cdc_test_sw\pad5_MB_MP_MT_0_0_10.a43" -v
This is the result when failing:
MSP Flasher v1.3.20
Evaluating triggers...done
Checking for available FET debuggers:
Found USB FET @COM10 <-Selected
Initializing interface @ COM10...done
Checking firmware compatibility:
FET firmware is up to date.
Reading FW version...done
Setting VCC to 3000 mV...done
Accessing device...done
Reading device information...done
Loading file into device...
Exit: 59
ERROR: Could not write device memory
Powering down...done Disconnecting from device...done
Driver :closed