This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sometimes this works and other times I get the ERROR 59. My computer is Windows 7. Using an MSP-FET tool.
This is what I'm running at the command prompt:
c:\ti\mspflasher_1.3.20\msp430flasher.exe -i COM10 -n "msp430F5419a" -w "c:\cdc_test_sw\pad5_MB_MP_MT_0_0_10.a43" -v
This is the result when failing:
MSP Flasher v1.3.20
Evaluating triggers...done
Checking for available FET debuggers:
Found USB FET @COM10 <-Selected
Initializing interface @ COM10...done
Checking firmware compatibility:
FET firmware is up to date.
Reading FW version...done
Setting VCC to 3000 mV...done
Accessing device...done
Reading device information...done
Loading file into device...
Exit: 59
ERROR: Could not write device memory
Powering down...done Disconnecting from device...done
Driver :closed
I have not tried the Uniflash. I was using an MSP-FET430UIF unit before this one with no problems.
Looked at the location in our code that was failing and this is what we had:
:1062C000090909090908080808080808070707074D
:0962D00007070707070707070786
:1062DA003140005C3C40001C3D401906B013A08FC1\
We saw that the Uniflash program was hesitating at address 0x62DA. Looking in the file we saw that a byte was missing so we put in an FF.
:1062C000090909090908080808080808070707074D
:0A62D000070707070707070707FF86
:1062DA003140005C3C40001C3D401906B013A08FC1
Uniflash does not hesitate at this address anymore and have not had any failures yet. I do not know why we never had this problem our older programmer (MSP-FET430UIF)
Hi Ernie,
So you are saying that the output file you are using to program the target is not supposed to have FF, but when you edited and inserted FF it now works???
I believe the error "cannot write device memory" is actually coming from the msp430 dll (MSP debug stack API) that MSP430Flasher and Uniflash use to control the MSP-FET HW.
What is your status now? Do you still need help?
Hi Dennis,
That is correct. I do not need the FF to run properly but it looks like it is needed to do the programming. We were thinking the same thing about the DLL.
I did the programming 10 times without any error. Before I would get 2 to 4 fails out of 10 tries. I was going to put this in my test program and run it today just to make sure there is no problem. I'm pretty sure this will work so I think I'm good.
Thanks for suggesting Uniflash as that gave us the exact location to look at.
**Attention** This is a public forum