Part Number: MSP430F5659
Other Parts Discussed in Thread: MSP430F5529
Hi,
I am working on MSP430F5659 controller, using USB developer package. I have implemented CDC for communication with PC.
For firmware upgrade, as mentioned USB developer package i am using "Python firmware upgrade GUI" which is HID tool.
Now i am able to load firmware on 1st time programming (fresh board) - i.e fresh board detect my board as HID device and i am able to load firmware.
For the second time and so on, i am pushing the device to BSL mode and i am able connect the device with "Python firmware upgrade GUI" tool, i.e on GUI opening and scanning i am getting
message "ready....."
On selecting user firmware(xyx.txt file) it starts mass erase and does the programming and prints "programming ok.". I am guessing this means a proper loading of firmware, am i correct?
After firmware upgrade using tool, i am seeing code changes are not working properly( i have done some pin configuration but its not working after firmware upgrade using tool, works well with JTAG programming)
Is there anything i need to do before i am building the my project, even i am seeing difference in .txt files for different build. ( i have the compiled the code in "Release mode")
Or whether this GUI is not supporting MSP430F5659 controller, please clarify.
Or any optimization issue causing this issue, Just a thought!!!!!!
Please help me in resolving this issue, Thanks in advance
Nitesh