Other Parts Discussed in Thread: MSP-FET, TEST2
Hi All,
We are facing some flashing related issue in a custom board of MSP430F5659. MCU flashed using MSP430 USB Firmware Upgrade V1.3.1, the TI-TXT file generated using CCS.
After Flashing it wont executing. We flashed the same using MSP-FET 430 JTAG in CCS but it works fine.
What might be the reasons for USB Firmware Upgrade wont work ?
Attaching the log of USB Firmware Upgrade :-
""" Starting
Password Sent Successfully
Sending RAM BSL v00.07.08.38
Done RAM BSL v00.07.08.38
Erasing memory segments
Sending C:\Users\name\Desktop\Application_test2.txt
Firmware Sent
Verifying memory
Memory successfully verified
Total programming time is 2s
Resetting Device...
Starting application
Done! """
Is the issue related to Boot Loader Version ? How can flash the Boot Loader to MCU ?
If the Boot Loader version changed can it reverted to old version ?
While Flashing Boot Loader , if a power failure is occurred can we revert it to back ?
Kindly Help !
Regards,
Renjith