Other Parts Discussed in Thread: ENERGIA, , MSP-FET
Below is the error I receive when I powered the device and open up Energia.
I am not able to load program to the board.
Energia: 1.6.10E18 (Windows 7), Board: "MSP-EXP430F5529LP"
Sketch uses 6,582 bytes (5%) of program storage space. Maximum is 131,072 bytes.
Global variables use 284 bytes (3%) of dynamic memory, leaving 7,908 bytes for local variables. Maximum is 8,192 bytes.
DSLite version 6.2.1.1595
Failed: MSP430: Error initializing emulator: MSP-FET / eZ-FET core(communication layer) update failed
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: MSP430
error: MSP430: Error initializing emulator: A firmware update is required for the MSP430 Debug Interface (MSP-FET430UIF / MSP-FET / eZ-FET). Click the "Update" button to update the firmware and launch your debug session (this may require several update steps). DO NOT UNPLUG THE INTERFACE DURING THE UPDATE.
Updating Firmware
Initializing Bootloader...
Programming New Firmware...
Programming New Firmware...: 75%
Programming New Firmware...: 84%
Programming New Firmware...: 91%
Programming New Firmware...: 100%
error: MSP430: Error: MSP-FET / eZ-FET core(communication layer) update failed
error: MSP430: Error: MSP-FET / eZ-FET core(communication layer) update failed
This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.
Please advise
Thanks,
Roland