This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am looking to design a simple motor control for a device similar to touch-less trash can lid/door opener, and hoping to get a recommendation for the right micro-controller.
The device will have two sensors and will control the motor to open/close the lid/door. I don't expect to have any embedded software involved in it, as the device is not complicated - one sensor makes the motor rotate in one direction and the other sensor for the other direction. The motor must stop when the lid/door opened or closed fully. The lid/door could be about 2 lbs in weight. The device is expected to operate just with battery or with DC converted from the home's main AC supply.
Can anyone recommend the right micro-controller for this kind of application or point me to any good sites to get related info/data,
Thanks
**Attention** This is a public forum