This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/MSP430-GCC-OPENSOURCE: GNU debugger internal error

Part Number: MSP430-GCC-OPENSOURCE
Other Parts Discussed in Thread: MSP430G2231, MSP430G2553

Tool/software: Linux

Hi,

I've just built the somnium maintained open-source compiler toolchain on Slackware 64 linux, using these two files:

msp430-gcc-6.2.1.16_source-full.tar.bz2

msp430-gcc-support-files-1.198.zip

Everything compiles without errors, and installs, and runs.   I am trying to set up msp430-gdb, to do debugging.

I can successfully set breakpoints, execute code, run the tui mode interface, etc.

But whenever I allow the program to run, and then try to interrupt it with a control signal, gdb crashes:

(gdb) c
Continuing.
^C
Remote connection closed
../../../gdb/gdb/value.c:1607: internal-error: value_free: Assertion `val->reference_count > 0' failed.
A problem internal to GDB has been detected,
further debugging may prove unreliable.
Quit this debugging session? (y or n) 

So, this is clearly a bug inside gdb itself, and likely has something to do with the somnium changes as gcc upgraded to version 6.6.1

Older tool-chains didn't crash on me.

I tried seeing if a bugfix already exists in the patches file:

msp430-gcc-6.2.1.16_source-patches.tar.bz2

However, the diffs are in "git diff" format; which I am unfamiliar with.  If I attempt to run standard linux "patch" on the files, patch complaints that at least some chunks are already applied and asks if I want to revert them.

So, I'm unsure if the source code already includes all the patches in  the source patches file, or not.  And I don't see an actual git repository address that I  can clone, to get  the most up to date source code and automate the patching process.

How are the open source compiler tools supported within  TI / how do I report a bug and get help ?

  • Andrew,

    This thread was sent over to us on the tools team. The guy that normally looks as the GNU related threads is out but will be back tomorrow. Reporting bugs with the GNU toolchain here on this forum is fine. We can work to reproduce and then work with Somnium if needed to resolve.

    Regards,
    John
  • Thanks, John.  


    If you need a core file, I believe I can generate one for gdb.  If you have a virtual box, I  can send you my binaries;  or I can allow a SSH login to a virtual machine if that would help  the team.

    If you are attempting to reproduce, and need more information, don't hesitate to ask.

    The following information ought to prove useful:

    I used compile instructions for gcc 5, from:  www.simplyembedded.org/.../compile-install-msp430-gcc  to build my binaries.  Note:  follow link to "updated instructions"

    My install directory is the only thing that differs, for I install to /opt/msp430/.local  and keep all source files in /opt/msp430/gcc2017

    I  also downloaded and compiled mspdebug-0.23.tar.gz with no special configuration options except my install  directory being /opt/msp430/.local

    To set up the debugger, I made a .gdbinit file and a msp430-gdbproxy.rc script, and a 69-ti-launchpad.rules for udev.

    I added myself to the dialout group on unix: as root: eg:    usermod -a -G dialout andrew3

    I then installed a udev rule (as root), called 69-ti-launchpad.rules to make the ti-launchpad USB driver allow dialout users to access the device.  The rule follows:

     

    ATTRS{idVendor}=="0451", ATTRS{idProduct}=="f432", MODE="0660", GROUP="dialout"

    Then I logged back in as andrew3 and I  plugged in  my ti launchpad, and executed "newgroup dialout"

    At this point, mspdebug rf2500 became completely operational.

    To make a script that can put mspdebug into proxy mode, I made the following  script:

    #!/bin/sh   
    # A script to put mspdebug into gdb proxy mode.
    # Alternately will download and flash a program, if program name is parameter
    if ps ax | grep -qe "mspdebug[^[]" ; then
    	echo "mspdebug already running gdb proxy mode."
    else
    	echo "Starting msp debug"
    	if [ -z "$1" ]; then
    		mspdebug rf2500 gdb 2>&1 > /dev/null &
    		disown
    		sleep 2
    	else
    		echo "prog $1" | mspdebug rf2500
    	fi
    
    fi

    And I made a gdb startup script, .gdbinit

    shell msp430-gdbproxy.rc
    set remoteaddresssize 64
    set remotetimeout 999999
    target remote localhost:2000
    enable tui
    layout src
    layout reg

    
    

  • I apologize for the delay.  The MSP430 GCC experts have been notified.

    Thanks and regards,

    -George

  • Hi Andrew,

    I haven't been able to reproduce this issue on Ubuntu 16.04 LTS.

    -bash $ sudo ./mspdebug rf2500 gdb
    MSPDebug version 0.23 - debugging tool for MSP430 MCUs
    Copyright (C) 2009-2015 Daniel Beer <dlbeer@gmail.com>
    This is free software; see the source for copying conditions.  There is NO
    warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
    Chip info database from MSP430.dll v3.3.1.4 Copyright (C) 2013 TI, Inc.
    
    Trying to open interface 1 on 027
    Initializing FET...
    FET protocol version is 30394216
    Set Vcc: 3000 mV
    Configured for Spy-Bi-Wire
    Device ID: 0x2553
      Code start address: 0xc000
      Code size         : 16384 byte = 16 kb
      RAM  start address: 0x200
      RAM  end   address: 0x3ff
      RAM  size         : 512 byte = 0 kb
    Device: MSP430G2xx3
    Number of breakpoints: 2
    fet: FET returned NAK
    warning: device does not support power profiling
    Chip ID data: 25 53
    Bound to port 2000. Now waiting for connection...
    Client connected from 127.0.0.1:56886
    Clearing all breakpoints...
    Running
    Target halted

    Running GDB with

    target remote :2000
    load
    continue

    does not cause the error you experience, the target continues and GDB stays connected as expected.

    The program being debugged is a simple empty main program. What is the program you are trying to debug?

    > Older tool-chains didn't crash on me.

    Do you mean older versions of msp430-elf-gdb, or that you don't see this error when building your project with older versions of GCC?

    > So, I'm unsure if the source code already includes all the patches in  the source patches file, or not. 

    The source-patches archive is essentially the diff between the msp430-gcc released version of gcc/newlib/binutils/gdb, and the upstream release of the given component number. e.g. if you clone the the upstream GCC repository, checkout to the tag corresponding to the release specified in the name of the diff file, and then apply the source-patches, the source code should be the same as that in the source-full package.

    >  If you have a virtual box, I  can send you my binaries

    If you could attach the binary that you are loading onto the target, that would be helpful. I can then see if I can reproduce. What is the specific msp430 device you are connecting to?

    > I used compile instructions for gcc 5, from:  www.simplyembedded.org/.../compile-install-msp430-gcc  to build my binaries.  Note:  follow link to "updated instructions"

    May I ask why you didn't build the package using the build script provided with the source-full package? Once you have the prerequisites, it's as simple as running "/bin/bash README.txt".

    What is the version of GCC used on your host system?

    Furthermore, is there a reason you want to build from source and aren't using the pre-built binary package provided. Does the problem reproduce with the pre-built binaries? We run the DejaGNU GDB testsuite before shipping the binaries, so we can be confident in their quality.

    Have you tried running GDB without your gdbinit script, and simply executing the program as I did above? Similarly, could you try with TUI disabled.

    Thanks,

  • Hi,

    I use a slackware64  system.  The library versions I  have are often  different  from Redhat or Ubuntu.  Historically, I have always had to build TI  toolchains from   source as prebuilt binaries will often not link.  Installing redhad or ubuntu  libraries to Slackware is a pain, so I avoid it when source code  is available.  The last toolchain  I built from TI was in late 2014 /  early 2015.  I do not recall GDB ever crashing at  that time, although many of it's features did not yet work.

    In  all previous versions of   the toolchain, readme.txt,  was not an  executable script and it's contents didn't  change from version to version.  When I opened   the readme.txt, I noted  that the top  of the  script says it's developed on CENTOS  7... and the dependencies  are controlled by yum.  Slackware doesn't have yum, apt get,   or rpm.  It's a purely script driven linux  system, similar to gentoo linux.   Since I am not familiar with  CENTOS, except that I thought  it was a windows clone, I didnt look at  the readme.txt further.

    The website link I gave you,  did the build of  the toolchain without use of any proprietary package manager,  and had an updated method for the latest version of GCC 6.2.  Therefore, that seemed like the most sure-fire way to build a proper  toolchain,  as he already had a working script.

    My hosts' GCC is version 5.3.0  

    I  am presently  compiling for  an MSP430g2231.  My  project directory  is called "source" and is attached to this   post.

    There  are more  than one compiler on the market, so that I have a macro library  to aid in porting from one C  compiler to the  next.  The "vector.h" file is  for C porting of the MSP430.

    I myself, however, have only compiled the code on  GCC  and  other compilers are not tested.

    NOTE: The TI website won't let me upload a .txz file as an attachment.  The  following discussion   is incorrect,  because I can't upload the binary.   How do I work around this issue?

    I have included my assembly language programing library called setisr.S which sets  the vector for an interrupt routine from assembly language.  The capital S extension allows the  C pre-processor and macro expansions to run on an assembly file.   This allows me to write  pure assembly language  programs for  the MSP430 series chips, without having to link in a C runtime library.  In the end,  assembly allows me to maximize chip usage.  setisr.S makes  programming interrupts very easy for me from  GNU Assembler,  which is why I wrote it.

    Instructions  for compiling each file, is  found in the comments of  the header.  I  have a generic "build" script which  merely  grep's the source file for  the gcc line, and executes it.  I am not including the build script in this tar archive.

    Inside the project directory you will find a.out.   That is the last binary I built from test7seg.S.  It  is an elf binary. You will also find "core" which I believe  is the last core  dump from GDB.

    My project is running a seven segment IO board, which is operates from  SPI bus, LS bit first, 16 bit  data.   There are two 74HCT shift and latch register chips, which take the SPI data and turn it into a scannable 7 segment display.    There are 4 digits on the  display, and so I scan  the common led line low for one of four digits,  while outputting an 8  bit character  which is seven segments plus a decimal point.  I also use the same 4 scan lines of the seven segment display, to scan input switches for a keyboard.

    The program is open loop with no error checking, so  it will  run even if no seven segment display is attached.

    To convert  from binary to BCD, to seven segment,  there is an assembly language function found  in bin2dec.S  that does the conversions.

    My original  project,  which  is not included here,  was a complete temperature/time controller for  a hot-plate and kilns. It measured resistance of the heating element  to estimate temperature, and regulated temperature in that way.

    My original project compiled on the older versions of GCC, which  predate TI's move to a new open source tool-chain maintainer.  I am rewriting  the code, and testing it fresh.

    I  used gdb to download the original firmware into my TI chip.  I don't recall gdb ever crashing on me  with the error message I  presently get.

    Whether  or not I  use TUI, I gdb still crashes.

    I have run gdb without the init script; but I  have never run it like you did, without setting   the remote message size.    I am not able to  test that right  now, but will try it later tonight.

  • Hi Andrew,

    I would encourage you to try the generic linux64 msp430 gcc package from the TI website: http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSPGCC/latest/index_FDS.html

    I would expect it to "just work" on most 64-bit linux systems, although I realise that you have more experience using your OS. The GCC package distributed from the TI website is configured for "x86_64-redhat-linux".

    I recognise that the error you are seeing is unlikely to be caused by a difference in how the toolchain is built, but it would be a good starting point if we are using the same toolchain. If the prebuilt package doesn't work, please try executing the README.txt script, as you probably have the prerequisites already if you have built the tools.

    Your project sounds like it consists of a lot of source files, a generic, reduced test case that can be built from a single source file would be appreciated. Can you clarify whether you see this error with a "barebones" project for your device, or if this is something you see only with your project.

    At this stage, without access to the elf file or source code I can't give any more help, I would suggest you upload them to a file sharing service and post the link here. We do not have the exact board you are using, the closest we have is the MSP430G2553, so if possible please build the project for this device. As I understand the G2553 is a similar, but superior chip to the G2231 so your project may just build for this device, unless you have lots of target-specific assembly code. This is another reason why a generic, reduced testcase would be useful.

    Thanks

**Attention** This is a public forum