Tool/software: Code Composer Studio
I am currently having problem with my code and am unable to detect whether there is some problem in configuration of the clock or configuration of RTC_B. It would be grateful if anybody provides help for resolving the issue and highlight the part I am missing out. I am providing my init functions for further referral
void vMspclock_init(void)
{
//-----------
//General Settings
UCSCTL6 &= ~(XT1OFF); // Enable XT1 for RTC_B
UCSCTL6 &= ~XT2OFF; // Enable XT2 for MCLK, SMCLK, ACLK
UCSCTL3 |= SELREF_2; // Reference to FLL is given from XT2
UCSCTL6 |= XT2DRIVE_3; //Selecting high current drive capacity and current consumption for 32 MHz crystal
//UCSCTL7 //This register is used to check oscillator fault flag, ie if there is some error in the osc due to supply conditions
//Init MCLK
UCSCTL4 |= SELM_5; //Uses XT2(32MHz) crystal oscillator source
UCSCTL5 |= DIVM_5; //Divides the clock source by 32, ie. 32/32 = 1Khz
//Init SMCLK
UCSCTL4 |= SELS_5; ////Uses XT2(32MHz) crystal oscillator source
UCSCTL5 |= DIVS_0; //Divides the clock source by 1, ie. 32/1 = 32Khz
//Init ACLK
UCSCTL4 |= SELA_5; ////Uses XT2(32MHz) crystal oscillator source
UCSCTL5 |= DIVA_3; //Divides the clock source by 8, ie. 32/8 = 4Khz
}
And function for init of RTC_B is
void init_RTC_B() //NO PRESCALER USED
{
// Setup Clock
UCSCTL6 &= ~(XT1OFF); // 32Mhz capacitor used for MCLK, SMCLK, ACLK
UCSCTL6 |= XCAP_3; // Cap 12pF configuration each
while(BAKCTL & LOCKBAK) // Unlock XT1 pins for operation
BAKCTL &= ~(LOCKBAK);
do
{
UCSCTL7 &= ~(XT1LFOFFG + DCOFFG);
// Clear XT1,DCO fault flags in case of possible faults that could set these registers high
SFRIFG1 &= ~OFIFG; // Clear oscillator fault flags
}while (SFRIFG1&OFIFG); // --------------------------------------------------------CODE IS STUCK HERE
RTCCTL0 |= RTCAIE; //Alarm interrupt for wake up from low power mode
//RTCAIFG is the interrupt register
RTCCTL1 |= RTCHOLD; //Disables the calender mode
RTCAMIN = 0x81;
RTCAHOUR = 0x00;
RTCHOUR = 0x5;//RTCHOUR = 0x5;
RTCMIN = 0x00;//RTCMIN = 0x00;
RTCSEC = 0x00;//RTCSEC = 0x00;
}
further information
1. XT1 is 32.768KHz and XT2 is 32MHz
2. I am using LPM3 and alarm interrupt in further code. Thanx