I am using an Olimex dev board https://www.olimex.com/Products/MSP430/Starter/MSP430-5510STK/ and a Silicon Labs CP2102 bridge on a USB stick. I'm using CCS 6.2.0, RealTerm to send over the serial port, and TI MSP-FET430UIF debugging interface. The board is being powered from the debugger.
I can't get the example UART code (MSP430F55xx_uscia0_uart_01.c) to run on it. I have tried the original code and tried modifying the baud rate. The receive interrupt is never triggered. I've put a scope on the TX from the PC, so I can clearly see that it is sending data. I have connected TX from the PC to RX on the MSP430 and vice versa. I've connected the ground from the bridge to the dev board ground. The MSP430 TX just sits at 3.3V.
I don't know how to move forward in debugging this.
Code below for reference. I changed the TX/RX pins to match the f5510.
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P4SEL |= BIT4+BIT5; // P4.4,5 = USCI_A0 TXD/RXD
UCA0CTL1 |= UCSWRST; // **Put state machine in reset**
UCA0CTL1 |= UCSSEL_2; // SMCLK
UCA0BR0 = 9; // 1MHz 115200 (see User's Guide)
UCA0BR1 = 0; // 1MHz 115200
UCA0MCTL |= UCBRS_1 + UCBRF_0; // Modulation UCBRSx=1, UCBRFx=0
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0, interrupts enabled
__no_operation(); // For debugger
}
// Echo back RXed character, confirm TX buffer is ready first
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA0IV,4))
{
case 0:break; // Vector 0 - no interrupt
case 2: // Vector 2 - RXIFG
while (!(UCA0IFG&UCTXIFG)); // USCI_A0 TX buffer ready?
UCA0TXBUF = UCA0RXBUF; // TX -> RXed character
break;
case 4:break; // Vector 4 - TXIFG
default: break;
}
}