This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/MSP-FET: Newer MSP-FET devices not working under Linux

Part Number: MSP-FET
Other Parts Discussed in Thread: MSP430-FLASHER, MSP-FLASHER, MSPDS

Tool/software: Linux

My issue is related to This Post. It seems that newer MSP-fet devices do not work under Linux. We ordered a new MSP-fet device (Serial number begins with 17 and ends with W).

In Linux (Lubuntu 15.10), using MSP430-Flasher  v1.3.8 we get the error "Could not set device VCC" (same symptom as described in the referenced post).

Updated MSP430-Flasher to v1.3.15 and ran the msp430uif_install.sh script from the Driver folder but still receive the same error (Could not set device VCC). 

Note that the Old MSP-Fet still works in Linux with MSP430-Flasher v1.3.15.

Interestingly, I found the following under Windows

New MSP-Fet: Using MSP430-Flasher v1.3.8: receive "Could not set device VCC" error (as expected)

New MSP-Fet: Using MSP430-Flasher v1.3.15 works properly (as expected)

Old MSP-Fet: Using MSP430-Flasher v1.3.8 works properly (as expected)

Old MSP-Fet: using MSP430-Flasher v1.3.15 Prompts for firmware upgrade (did not do this in Linux). I said no for fear that doing so would prevent it from working under Linux, then received "Could not set device VCC" error.

I would like to be able to use either device under either OS, but at the very least, the new MSP-fet should work with the new MSP430-Flasher under Linux.

Thanks.

**Attention** This is a public forum