This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
I have doubts on the way figure 1 of the datasheet (safe operating area) should be understood:
my customer operates at 3.3V 16MHz and has flash corruption problem. He's investigating if slight drops on Vcc can happen.
If Vcc drops at 3.2V operating at 16MHz:
- do we guarantee CPU execution?
- do we guarantee flash write/erase?
thanks
Part Number: MSP430G2553
team,
Is there a constraint of vcc min vs Fftg max or can customer program the ISP the way she/he like withing Vcc 2.2/3.6V - Fftg 257/476KHz ?
thanks
Hi!
According to the datahseet, the minimum supply voltage for 16MHz is 3.3V - if you cannot maintain 3.3V, running the device at 16MHz might not be the best idea, although I think that it will work at 3.2V, but the datasheet is the document to stick to when designing serious electronics. However, the flash write works down to a supply voltage of 2.2V, so no problem here. What is your customer's prescaler for the flash controller clock?
Dennis
**Attention** This is a public forum