This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
Till now we worked with TIs MSP compiler. But to include BG Library for controlling silicon labs BLE121LR BLE module, we shifted to use MSP430 GCC compiler. As we changed the compiler we are getting the below errors:
1.
Description Resource Path Location Type
undefined reference to `_delay_cycles' main.c /BLE_MSP_3 C/C++ Problem
For this instead of using _delay_cycles I started using below code which I found from web.
void brief_pause(register unsigned long n)
{
__asm__ __volatile__ (
"1: \n"
" dec %[n] \n"
" jne 1b \n"
: [n] "+r"(n));
}
I commented and removed all the _delay_cycles but still getting the same above error.
2.
Description Resource Path Location Type
undefined reference to `pow' main.c /BLE_MSP_3 C/C++ Problem
Please suggest me relavant function to use instead of pow
3.
Description Resource Path Location Type
BLE_MSP_3.out section `.text' will not fit in region `ROM' BLE_MSP_3 C/C++ Problem
I am not getting why this error is coming.
4.
Description Resource Path Location Type
Dwarf Error: mangled line number section. BLE_MSP_3 C/C++ Problem
5.
Description Resource Path Location Type
region `ROM' overflowed by 12692 bytes BLE_MSP_3 C/C++ Problem
We migrated to MSP430 GCC compiler without much changes in the code. Please suggest me if any measures to be taken before migrating.
Thanks in advance.
**Attention** This is a public forum