This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Is there any way to migrate an existing CCS project from SimpleLink SDK 1.40.01.00 to 1.50.00.12?
CCS is just telling me:
Product 'com.ti.SIMPLELINK_MSP432_SDK' v1.40.1.00 is not currently installed and no compatible version is available. Please install this product or a compatible version.
Build stopped..
Update:
This can be found in the release notes as well as in the Resource Explorer documentation:
Tobias,
In the CCS project properties there is a products tab (Properties->General). You should see the available simplelink SDKs there. Select the SDK you wish to use.
Your include options should be relative paths based upon the SDK.
Which is defined automatically in the Path Variables when you select the SDK.
Let me know if you have any questions or if you are not seeing these windows/parameters.
Chris
**Attention** This is a public forum