This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-EXP432P401R
I am implementing 3-phase energy metering with requirements to have data storage up to one month, wireless and web browser as well, accuracy for U and I measurement 0.2% (>12 bits of resolution), 32 digital I/O and so on. In addition, isolation amplifiers AMC1301 (sigma-delta modulation, differential output) will be used.
I have a doubt which LaunchPad to use, whether MSP430FR5994 (12-bit ADC, SD slot built-in, external ADCs needed to achieve required accuracy) or MSP432P401R (14-bit ADC, no SD slot). According to your experience, which approach could cause more obstacles during implementation? If you also have any other advice, I will be very thankful.
Thank you in advance,
Adi
**Attention** This is a public forum