I look for the Technical Reference Manual about Comparator E Module,and the registers CExCTL1 says
CEIES = 0 is rsing edge and CEIES = 1 is falling edge,
but when it goes to the driverLib code of comp_e.c
|
1
2
3
4
5
6
7
8
9
10
11
|
void COMP_E_setInterruptEdgeDirection(uint32_t comparator, uint_fast8_t edgeDirection) { ASSERT(edgeDirection <= COMP_E_RISINGEDGE); // Set the edge direction that will trigger an interrupt if (COMP_E_RISINGEDGE == edgeDirection) BITBAND_PERI(COMP_E_CMSIS(comparator)->CTL1, COMP_E_CTL1_IES_OFS) = 1; else if (COMP_E_FALLINGEDGE == edgeDirection) BITBAND_PERI(COMP_E_CMSIS(comparator)->CTL1, COMP_E_CTL1_IES_OFS) = 0; } |
the CEIES = 1 is rising edge and CEIES = 0 is falling edge?
Am i wrong or the code is wrong?