Part Number: MSP432P401R
Other Parts Discussed in Thread: ENERGIA, PCF8574, P82B96
Tool/software: Code Composer Studio
Hi, Guys
I found this code in E2E and seems this person has successfully used this code to interface with his LCD screen. However I downloaded his code and compiled into my Launchpad and it does not seems to work. Could really use some help with this. I have attached the code. Although I could interface LCD through Energia, but I really wants to use code composer studio.
/*****************************************************************/
/********* *********/
/********* AUTOR: ANTONIO ARMANDO BIZA FERREIRA *********/
/********* PROJECTO: ECG *********/
/********* DATA: 01-02-2017 *********/
/********* IDE: CODE COMPOSER STUDIO V6.2 *********/
/********* MCU: MSP432 *********/
/********* *********/
/********* FILE: MAIN.C *********/
/********* *********/
/*****************************************************************/
#include <msp432.h>
#include "main.h"
#include "lcd.h"
void main(void)
{
volatile uint32_t i;
WatchDogHold();
LCD_PortConfig();
LCD_Initialize();
APP_Initialize();
while(1){
}
}
void APP_Initialize(void){
LCD_SetText("TESTING",3 ,0);
}
void WatchDogHold(void){
WDTCTL = WDTPW | WDTHOLD; /*STOP WATCHDOG TIMMER*/
}
/*****************************************************************/
/********* *********/
/********* AUTOR: ANTONIO ARMANDO BIZA FERREIRA *********/
/********* PROJECTO: ECG *********/
/********* DATA: 01-02-2017 *********/
/********* IDE: CODE COMPOSER STUDIO V5 *********/
/********* MCU: MSP432 *********/
/********* *********/
/********* FILE: LCD.H *********/
/********* *********/
/*****************************************************************/
/*****************************************************************/
/********* INCLUDE *********/
/*****************************************************************/
#include "lcd.h"
/*****************************************************************/
/********* DEFINES *********/
/*****************************************************************/
#define EN (PORT2 + BIT3)
#define RS (PORT6 + BIT7)
#define D4 (PORT2 + BIT6)
#define D5 (PORT2 + BIT4)
#define D6 (PORT5 + BIT6)
#define D7 (PORT6 + BIT6)
/*COMMAND*/
#define CLEAR 0x01
/*****************************************************************/
/********* LOCAL FUNCTIONS *********/
/*****************************************************************/
/*LCD PIN OUT DIRECTION*/
void lcdDirPinOut(unsigned int pin){
if((pin & 0xFF00) == PORT2){
P2DIR |= (pin & 0x00FF);
}else if((pin & 0xFF00) == PORT5){
P5DIR |= (pin & 0x00FF);
}else{
P6DIR |= (pin & 0x00FF);
}
}
/*LCD PIN OUT SET*/
void lcdSetPinOut(unsigned int pin){
if((pin & 0xFF00) == PORT2){
P2OUT |= (pin & 0x00FF);
}else if((pin & 0xFF00) == PORT5){
P5OUT |= (pin & 0x00FF);
}else{
P6OUT |= (pin & 0x00FF);
}
}
/*LCD PIN OUT CLR*/
void lcdClrPinOut(unsigned int pin){
if((pin & 0xFF00) == PORT2){
P2OUT &= ~(pin & 0x00FF);
}else if((pin & 0xFF00) == PORT5){
P5OUT &= ~(pin & 0x00FF);
}else{
P6OUT &= ~(pin & 0x00FF);
}
}
void lcdSetValue(unsigned char value){
if(value & 0x08){
lcdSetPinOut(D7);
}else{
lcdClrPinOut(D7);
}
if(value & 0x04){
lcdSetPinOut(D6);
}else{
lcdClrPinOut(D6);
}
if(value & 0x02){
lcdSetPinOut(D5);
}else{
lcdClrPinOut(D5);
}
if(value & 0x01){
lcdSetPinOut(D4);
}else{
lcdClrPinOut(D4);
}
delay_us(5);
}
void lcdTriggerEN(){
lcdSetPinOut(EN);
delay_us(5);
lcdClrPinOut(EN);
// delay_us(5);
}
void lcdWriteData(unsigned char data){
lcdSetPinOut(RS); // Set RS to Data
lcdSetValue(data >> 4); // Upper nibble
lcdTriggerEN();
lcdSetValue(data); // Lower nibble
lcdTriggerEN();
delay_us(30); // Delay > 50 us
}
void lcdWriteCmd(unsigned char cmd){
lcdClrPinOut(RS); // Set RS to Cmd
lcdSetValue(cmd >> 4); // Upper nibble
lcdTriggerEN();
lcdSetValue(cmd); // Lower nibble
lcdTriggerEN();
delay_ms(2); // Delay > 5ms
}
/*****************************************************************/
/********* GLOBAL FUNCTIONS *********/
/*****************************************************************/
/*
*
*/
void LCD_PortConfig(void)
{
// Direction
lcdDirPinOut(D4);
lcdDirPinOut(D5);
lcdDirPinOut(D6);
lcdDirPinOut(D7);
lcdDirPinOut(EN);
lcdDirPinOut(RS);
}
/*
*
*/
void LCD_Initialize(void)
{
/* delay_us(80);
lcdWriteCmd(0x28); // 4-bit, 2 line, 5x8
P2OUT = 0x03; // Start LCD (send 0x03)
lcdTriggerEN(); // Send 0x03 3 times at 5ms then 100 us
delay_ms(2);
lcdTriggerEN();
delay_ms(2);
lcdTriggerEN();
delay_ms(2);
lcdWriteCmd(0x28); // 4-bit, 2 line, 5x8
P2OUT = 0x02; // Switch to 4-bit mode
lcdTriggerEN();
delay_ms(2);*/
lcdWriteCmd(0x28); // 4-bit, 2 line, 5x8
lcdWriteCmd(0x08); // Instruction Flow
lcdWriteCmd(0x01); // Clear LCD
lcdWriteCmd(0x06); // Auto-Increment
lcdWriteCmd(0x0C); // Display On, No blink
}
void LCD_SetText(char* text, int x, int y){
unsigned int i;
if (x < 16) {
x |= 0x80; // Set LCD for first line write
switch (y){
case 1:
x |= 0x40; // Set LCD for second line write
break;
case 2:
x |= 0x60; // Set LCD for first line write reverse
break;
case 3:
x |= 0x20; // Set LCD for second line write reverse
break;
}
lcdWriteCmd(x);
}
i = 0;
while (text[i] != '\0') {
lcdWriteData(text[i]);
i++;
}
}
void LCD_SetInt(int val, int x, int y)
{
char number_string[16];
sprintf(number_string, "%d", val); // Convert the integer to character string
LCD_SetText(number_string, x, y);
}
void LCD_Clear()
{
lcdWriteCmd(CLEAR);
}
void LCD_LoadSymbols(void)
{
int j;
static char empty[] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
static char heart[] = {0x00, 0x0A, 0x1F, 0x1F, 0x1F, 0x0E, 0x04, 0x00};
static char bat_100[] = {0x0E, 0x1F, 0x1F, 0x1F, 0x1F, 0x1F, 0x1F, 0x1F};
static char bat_75[] = {0x0E, 0x1F, 0x11, 0x1F, 0x1F, 0x1F, 0x1F, 0x1F};
static char bat_50[] = {0x0E, 0x1F, 0x11, 0x11, 0x11, 0x1F, 0x1F, 0x1F};
static char bat_25[] = {0x0E, 0x1F, 0x11, 0x11, 0x11, 0x11, 0x1F, 0x1F};
static char bat_0[] = {0x0E, 0x1F, 0x11, 0x11, 0x11, 0x11, 0x11, 0x1F};
lcdWriteCmd(0x40);
for(j=0;j!=8;j++){
lcdWriteData(empty[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(heart[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(bat_100[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(bat_75[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(bat_50[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(bat_25[j]);
}
for(j=0;j!=8;j++){
lcdWriteData(bat_0[j]);
}
lcdWriteCmd(CMD_END);
}
void LCD_SetSymbol(unsigned char symbol, unsigned char offset, unsigned char line)
{
lcdWriteCmd(line+offset);
lcdWriteData(symbol);
}