This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
This code successfully gets 10 pulse readings from the pulse sensor, but I'm trying to write code that will find the time between the max/peak pulses so I can calculate heart beats per minute. Can anyone help me write
this code, because I'm really struggling. The pulse sensor gives out an analog value of about 500 when nobody is touching the sensor, but when somebody is touching the sensor, a peak value is about 700 - which indicates a heart beat.
Can anybody help me write this code?
#include "msp430g2253.h" // Variables int adc[50] = {0}; //Sets up an array of 10 integers and zero's the values int avg_adc = 0; // Function prototypes void adc_Setup(); void adc_Sam10(); void main() { WDTCTL = WDTPW + WDTHOLD; // Stop WDT adc_Setup(); // Fucntion call for adc_setup while(1) { long adctot = 0; adc_Sam10(); // Function call for adc_samp // Add all the sampled data and divide by 10 to find average int i = 0; for(i = 0; i <= 49; i++){ adctot = adctot + adc[i]; } avg_adc = adctot/50; } } // ADC10 interrupt service routine #pragma vector=ADC10_VECTOR __interrupt void ADC10_ISR(void) { __bic_SR_register_on_exit(CPUOFF); // Clear CPUOFF bit from 0(SR) } // ADC set-up function void adc_Setup() { ADC10CTL1 = CONSEQ_2 + INCH_0; // Repeat single channel, A0 ADC10CTL0 = ADC10SHT_2 + MSC + ADC10ON + ADC10IE; // Sample & Hold Time + ADC10 ON + Interrupt Enable ADC10DTC1 = 0x32; // 1000 conversions ADC10AE0 |= 0x01; // P1.0 ADC option select } // ADC sample conversion function void adc_Sam10() { ADC10CTL0 &= ~ENC; // Disable Conversion while (ADC10CTL1 & BUSY); // Wait if ADC10 busy ADC10SA = (int)adc; // Transfers data to next array (DTC auto increments address) ADC10CTL0 |= ENC + ADC10SC; // Enable Conversion and conversion start __bis_SR_register(CPUOFF + GIE);// Low Power Mode 0, ADC10_ISR }
**Attention** This is a public forum