Part Number: MSP430F47197
Other Parts Discussed in Thread: MSP430F47127
Dear All,
I am trying to set baud rate on MSP430F47127 and having problem.
Clock = 4194304
SCFI0 = FLLD_4+FN_4;
SCFQCTL = 31; // (31+1) * 32768 * 4 = 4194304
I am trying to set baud to 9600
P1SEL |= BIT6+BIT7; // P1.6,7 = USCI_A1 RXD/TXD
UCA1CTL1 |= UCSSEL_2; // CLK = SMCLK
UCA1BR0 = 0xB4;
UCA1BR1 = 0x01;
UCA1MCTL = 0xDF;
UCA1CTL1 &= ~UCSWRST; // Initialize USCI state machine
UC1IE |= UCA1RXIE ; // Enable USCI_A0 RX interrupt
But it is not working.
I have also tried :
P1SEL |= BIT6+BIT7; // P1.6,7 = USCI_A1 RXD/TXD
UCA1CTL1 |= UCSSEL_1; // CLK = ACLK
UCA1BR0 = 0x03;
UCA1BR1 = 0x00;
UCA1MCTL = 0x29;
UCA1CTL1 &= ~UCSWRST; // Initialize USCI state machine
UC1IE |= UCA1RXIE ; // Enable USCI_A0 RX interrupt
But unfortunately it also not working.
However when I tried to set to 19200 baud rate, it worked.
P1SEL |= BIT6+BIT7; // P1.6,7 = USCI_A1 RXD/TXD
UCA1CTL1 |= UCSSEL_2; // CLK = SMCLK UCSSEL_2
UCA1BR0 = 0xDA;
UCA1BR1 = 0x00;
UCA1MCTL = 0xAA;
UCA1CTL1 &= ~UCSWRST; // Initialize USCI state machine
UC1IE |= UCA1RXIE ; // Enable USCI_A0 RX interrupt
But i need to set it on 9600 baud rate. Please help.
Thanks in advance.