This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430G2553: Can one debug while configured for hardware UART on g2553 launchpad?

Part Number: MSP430G2553

Tool/software: Code Composer Studio

Hi,

I've searched and haven't found a definitive answer to this question. I have a working program which outputs ascii through UART, on ports 1.1 and 1.2.

I have configured the jumpers on the launchpad to use hardware UART, and have managed to see output in the CCS terminal window. 

However, I lose connectivity with the FET configured this way, meaning I can no longer update or debug code. I've tried numerous combinations of COM ports, but still no joy.

Am I missing something really obvious?

Edit: this is on CCS6, Windows 10

TIA

**Attention** This is a public forum