This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Hi,
i try to get the BSL running with invocation through my application software.
I got a board with a MAX3386E RS232 converter on it connected to eUSCI_A0. According to SLAU622G section 3.3.1 it's possible.
I've included the following code into my application software, which is called by a command over the serial connection.
#include "msp.h" #include <ti/devices/msp432p4xx/driverlib/driverlib.h> ... #define BSL_PARAM 0xFC48DFFF // I2C slave address = 0x48, Interface selection = UART //#define BSL_API_TABLE_ADDR 0x00202000 // Address of BSL API table #define BSL_ENTRY_FUNCTION (*((uint32_t *)BSL_API_TABLE_ADDR)) ... main() { ... if (status & STATUS_BSL) { status &= ~STATUS_BSL; MAP_Interrupt_disableMaster(); NVIC->ICER[0] = 0xFFFF; NVIC->ICPR[0] = 0xFFFF; NVIC->ICER[1] = 0xFFFF; NVIC->ICPR[1] = 0xFFFF; ((void (*)())BSL_ENTRY_FUNCTION)((uint32_t)BSL_PARAM); // Call the BSL with given BSL parameters } ... }
When i now try to enter the BSL, the MCU leaves my application software ( doesn't respond to my commands on the serial) but the BSL_scripter can't establish a connection to the device. With a scope i can see the Signals comming from the Scripter, but no answer from the device.
When i use a brand-new MCU or a Device which got reset to factory defaults, it works.
The BSL_Scripter ist startet out of a cmd-window like the following
C:\EigeneDaten\Workspace_v7\Datenlogger\Debug>C:\EigeneDaten\Datenblaetter_u_sonstiges\MSP_Doku\MSPBSL_Scripter_win\BSL-Scripter.exe -d -g -n P4xx -i [COM1,UART,9600,PARITY] -b -z [RESET] --------------------------------------------------------- BSL Scripter 3.3.0 PC software for BSL programming 2018-Apr-27 10:50:22 --------------------------------------------------------- Log mode is turned off! C:\EigeneDaten\Datenblaetter_u_sonstiges\MSP_Doku\MSPBSL_Scripter_win\BSL-Scripter.exe -d -g -n P4xx -i [COM1,UART,9600,PARITY] -b -z [RESET] Verbose is turned on! Device : P4xx Init communication parameters : [COM1,UART,9600,PARITY] [ERROR_MESSAGE]Initialization of P4xx BSL failed! Exit the scripter!
I got no idea left why it does not work correctly.
Regards
Thomas
Hi Chris,
the delay between invocation and communication with BSL is approximately 2 seconds.
I also tried the auto-setting without any success.
In the msp432p401r.cmd where all the Memorie-Sections are listet i only added 2 sections for data and config starting at 0x0003 B000 with a total length of 0x0000 4000.
I didn't change anything at the section called INFO, where the BSL ist located.
When i use memory browser and take a look at the adress of the BSL (0x0020 2000), it seems to be alright.
Is there a possibility to Flash a clean new BSL into the device in case somehow something chnaged one byte in the BSL-Code?
Regards,
Thomas
As additional information:
When i read the MCU with TX_DATA_BLOCK_32 starting at the adress 0x00e8 with a length of 64532 bytes, i get the correct code.
When doing a CRC_CHECK_32 starting at 0x00e8 with a length of 16 bytes, the result is as expected.
Another try with an intel-hex-file is also not working.
Where can i readback the Size of my written firmware in css?
Regards,
Thomas
Hi,
i'm still trying to get the BSL working.
Now i'm not able to flash any of my own programs to the mcu. A fresh programmed BSL with uniflash changes nothing. The blink.txt example works fine.
I also tried to use the BSL with the MSP432 LaunchPad, which doesn't work also.
I reduced my firmware to a minimum (Ti-TXT-file from 192kB reduced to 29kB) to verify that the size does not matter without any success. I get the same verification error and the firmware does not run.
What must be considered in the settings of CCS?
Regards,
Thomas
EDIT: May it help when i send the firmware-file to a TI-employee?
Thomas,
I do not see any issue with you code, but I will ask a colleague to also look at it. Can you also provide the script that the BSL scriptor is using as well as the .txt/.hex file that is being downloaded? You mention that it works once with a newly flashed BSL, which leads me to believe that the BSL itself is being overwritten.
Also, can you explain the flow of the BSL update? You have the code that you provided which invokes the BSL and then the firmware update takes place. Does the firmware update contain another software BSL invocation which is not working? Or are you reflashing the same program and then the software BSL invocation does not work.
I will be able to run your code tomorrow with the blink LED example found in the BSL scripter and let you know if I am successful.
Regards,
Chris
Hello Thomas,
I acknowledge this behaviour. There was a bug in 3.3.0 and been fixed in 3.4.0 that just released last week.
It would be great if you could tested with the new version and let me know the result.
Hello,
this version does not work the same way the version 3.3.0. I took the simple example i posted befor and used the button on P1.1 to invoke the BSL on the launchpad. Within the 10s timeout i started the scripter with the following command-line:
BSL-Scripter.exe -d -n P4xx -i [COM2,UART,9600,PARITY] -b -w BSL_TEST.txt -v -z [RESET]
This didn't work.
I flashed a new BSL to the launchpad using uniflash and started the scripter the same way. This worked and the led P1.0 started to blink like programmed. i invoked the bsl on launchpad again (button P1.1) and started the scripter with the same parameters and it returned with an initialization error.
Thsi is the ti-txt-file i try to flash into the mcu
@0000 00 00 01 20 33 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 3F 0C 00 00 3F 0C 00 00 00 00 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 0B 01 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 3F 0C 00 00 08 B5 C6 48 00 68 00 6A 01 46 C5 48 88 47 C5 48 00 68 C0 68 01 21 02 46 01 20 90 47 C2 49 08 68 40 1C 08 60 08 BD 08 B5 BE 48 00 68 C0 68 01 21 02 46 02 20 90 47 BB 48 00 68 40 6B 02 21 02 46 01 20 90 47 B9 49 04 20 08 70 08 BD 08 B5 B5 48 00 68 00 68 FF 21 02 46 01 20 90 47 B1 48 00 68 00 68 FF 21 02 46 02 20 90 47 AE 48 00 68 00 68 FF 21 02 46 03 20 90 47 AA 48 00 68 00 68 FF 21 02 46 04 20 90 47 A7 48 00 68 00 68 FF 21 02 46 05 20 90 47 A3 48 00 68 00 68 7F 21 02 46 06 20 90 47 A0 48 00 68 00 68 FF 21 02 46 07 20 90 47 9C 48 00 68 00 68 FF 21 02 46 08 20 90 47 99 48 00 68 00 68 FF 21 02 46 09 20 90 47 95 48 00 68 00 68 FF 21 02 46 0A 20 90 47 92 48 00 68 80 68 FF 21 02 46 01 20 90 47 8E 48 00 68 80 68 FF 21 02 46 02 20 90 47 8B 48 00 68 80 68 FF 21 02 46 03 20 90 47 87 48 00 68 80 68 FF 21 02 46 04 20 90 47 84 48 00 68 80 68 FF 21 02 46 05 20 90 47 80 48 00 68 80 68 FF 21 02 46 06 20 90 47 7D 48 00 68 80 68 FF 21 02 46 07 20 90 47 79 48 00 68 80 68 FF 21 02 46 08 20 90 47 76 48 00 68 80 68 FF 21 02 46 09 20 90 47 72 48 00 68 80 68 FF 21 02 46 0A 20 90 47 72 49 FF 20 08 80 71 49 00 20 08 80 71 49 30 20 08 80 70 49 00 20 08 80 69 48 00 68 C0 69 01 22 03 21 03 46 0B 20 98 47 65 48 00 68 40 69 02 21 02 46 01 20 90 47 61 48 00 68 40 6B 02 21 02 46 01 20 90 47 5E 48 00 68 40 6A 02 21 01 22 03 46 01 20 98 47 5A 48 00 68 80 6A 02 21 02 46 01 20 90 47 5D 48 00 68 80 69 01 46 33 20 88 47 08 BD 10 B5 50 48 00 68 00 68 04 46 4F 48 04 21 01 22 01 23 A0 47 4C 48 00 68 55 49 80 68 02 46 4A 48 90 47 48 48 00 68 51 49 40 68 02 46 47 48 90 47 50 49 29 20 00 F0 91 FC 43 48 00 68 00 6A 01 46 42 48 88 47 40 48 00 68 80 69 01 46 3F 48 88 47 3D 48 00 68 00 69 02 46 3C 48 00 21 90 47 10 BD 08 B5 44 48 00 68 00 68 80 47 FF F7 04 FF 4F F4 00 40 00 21 00 F0 45 FC 03 20 00 F0 8A FC 3E 48 00 68 00 68 00 21 00 22 03 46 4F F0 80 50 98 47 3A 48 00 68 00 68 00 21 00 22 03 46 01 20 98 47 36 48 00 68 00 68 03 21 00 22 03 46 08 20 98 47 32 48 00 68 00 68 03 21 00 22 03 46 02 20 98 47 2E 48 00 68 00 68 03 21 00 22 03 46 04 20 98 47 FF F7 96 FF 25 48 00 68 00 68 80 47 00 BF 1D 48 00 78 00 21 00 B1 01 21 00 29 F7 DD 18 48 00 68 C0 68 02 21 02 46 02 20 90 47 16 49 00 20 08 70 1A 48 00 68 40 68 80 47 1D 49 4F F6 FF 70 08 60 1C 49 4F F6 FF 70 08 60 1B 49 4F F6 FF 70 08 60 1A 49 4F F6 FF 70 08 60 19 49 4F F6 FF 70 08 60 18 49 4F F6 FF 70 08 60 17 48 00 68 01 46 16 48 88 47 CB E7 C0 46 5C 08 00 02 00 C0 00 40 24 08 00 02 FC 00 00 20 00 01 00 20 24 4D 00 40 22 4D 00 40 2A 4D 00 40 2C 4D 00 40 2C 08 00 02 36 6E 01 00 E5 00 00 00 64 08 00 02 14 08 00 02 80 E1 00 E0 80 E2 00 E0 84 E1 00 E0 84 E2 00 E0 00 E3 00 E0 04 E3 00 E0 00 20 20 00 FF FF 48 FC AD F1 20 0D 00 20 00 90 00 20 01 90 00 20 02 90 00 20 03 90 00 20 04 90 00 20 AD F8 18 00 AC 48 05 90 AC 48 00 68 00 F4 E0 20 00 0C 01 90 01 99 01 20 88 40 02 90 A7 48 00 68 00 F0 07 00 00 90 06 E1 A5 48 00 78 48 B3 A4 49 46 F6 5A 10 08 60 A3 49 08 68 40 F0 01 00 08 60 A0 49 01 20 08 60 9D 48 00 78 90 B1 9F 48 00 78 38 B1 02 98 9E 49 4F F4 FA 32 B2 FB F0 F0 08 60 FB E0 02 98 9A 49 4F F4 FA 42 B2 FB F0 F0 08 60 F3 E0 02 98 96 49 4F F4 00 42 B2 FB F0 F0 08 60 EB E0 02 98 92 49 4F F4 00 42 B2 FB F0 F0 08 60 E3 E0 02 98 8E 49 42 F2 10 72 B2 FB F0 F0 08 60 DB E0 89 48 00 78 38 B1 02 98 88 49 4F F4 FA 32 B2 FB F0 F0 08 60 D0 E0 02 98 84 49 4F F4 FA 42 B2 FB F0 F0 08 60 C8 E0 82 48 00 68 6F F3 9F 20 AD F8 18 00 11 E0 7F 48 03 90 22 E0 7F 48 03 90 1F E0 7E 48 03 90 1C E0 7E 48 03 90 19 E0 7D 48 03 90 16 E0 7D 48 03 90 13 E0 75 48 00 68 10 F4 E0 20 E8 D0 B0 F5 80 30 E8 D0 B0 F5 80 30 E8 D0 B0 F5 80 30 E8 D0 B0 F5 80 30 E8 D0 B0 F5 80 30 E8 D0 BD F9 18 00 18 B9 03 98 68 49 08 60 94 E0 BD F9 18 00 40 0B 05 D3 BD F9 18 00 40 F4 70 40 AD F8 18 00 6A 48 00 78 30 B1 69 48 00 68 05 90 69 48 00 68 04 90 05 E0 68 48 00 68 05 90 67 48 00 68 04 90 04 98 DD ED 05 0A C0 F5 40 70 00 EE 10 0A B8 EE 40 1A B7 EE 00 0A 01 EE 20 0A DD ED 05 0A BD F9 18 00 01 EE 10 0A F2 EE 00 1A B8 EE C1 1A 20 EE 21 0A 61 EE 20 0A 80 EE 80 0A 03 98 00 EE 90 0A B7 EE 00 1A F8 EE 60 0A 31 EE 40 0A 80 EE 80 0A BC EE C0 0A 45 49 10 EE 10 0A 08 60 4B E0 02 9A 48 48 41 49 B0 FB F2 F0 08 60 44 E0 4C 48 00 78 40 B3 3A 49 46 F6 5A 10 08 60 39 49 08 68 40 F0 02 00 08 60 36 49 01 20 08 60 44 48 00 78 90 B1 35 48 00 78 38 B1 02 98 34 49 4F F4 FA 32 B2 FB F0 F0 08 60 27 E0 02 98 30 49 4F F4 FA 42 B2 FB F0 F0 08 60 1F E0 02 9A 33 48 2B 49 B0 FB F2 F0 08 60 18 E0 02 9A 2F 48 28 49 B0 FB F2 F0 08 60 11 E0 00 98 00 28 3F F4 F5 AE 40 1E 3F F4 27 AF 40 1E 3F F4 2C AF 40 1E 3F F4 3C AF 40 1E B6 D0 40 1E BB D0 FF E7 08 B0 70 47 29 49 08 68 40 F4 70 00 08 60 28 49 4F F4 B5 40 08 80 27 49 80 20 08 60 12 49 46 F6 5A 10 08 60 14 49 4F F4 80 30 08 60 0C 48 0C 49 00 68 20 F0 07 10 40 F0 03 00 08 60 0A 49 00 20 08 60 1D 48 1C 49 00 68 20 F0 30 00 08 60 1B 48 1A 49 00 68 20 F0 30 00 08 60 70 47 00 00 00 00 08 04 01 40 00 89 20 42 00 04 01 40 50 04 01 40 3C 86 20 42 08 01 00 20 04 04 01 40 60 E3 16 00 C0 C6 2D 00 80 8D 5B 00 00 1B B7 00 00 36 6E 01 00 6C DC 02 D8 80 20 42 84 10 20 00 6C 10 20 00 64 10 20 00 4C 10 20 00 04 89 20 42 88 ED 00 E0 0C 48 00 40 14 30 04 E0 10 10 01 40 14 10 01 40 2D E9 F8 43 23 4F 05 46 46 F6 5A 10 0C 46 38 60 00 F0 32 FA 00 F0 01 09 01 20 00 F0 1D FA 00 20 B5 F5 00 7F 08 BF 01 20 84 46 00 20 04 B1 01 20 80 46 19 48 B5 F5 00 7F 08 D0 F9 68 00 23 41 F0 03 01 F9 60 01 26 80 F8 A4 31 02 E0 01 26 80 F8 A4 61 80 F8 A0 61 01 E0 80 F8 00 6A 90 F8 00 39 23 B1 B8 F1 00 0F F7 D0 64 1E F5 D1 BC F1 01 0F 04 D0 F9 68 21 F0 03 01 0D 43 FD 60 06 70 48 46 00 F0 F2 F9 30 46 B8 F1 01 0F 04 BF 00 2C 00 20 BD E8 F8 83 00 04 01 40 00 80 20 42 00 2A 4A D0 5F EA 00 0C 8B 07 1C D1 83 07 22 D1 10 2A 08 D3 70 B4 10 3A 78 C9 78 C0 10 3A FB D2 70 BC 10 32 38 D0 04 2A 2C D3 08 2A 05 D3 0C 2A 24 BF 08 C9 08 C0 08 C9 08 C0 08 C9 08 C0 92 07 2A D0 92 0F 22 E0 0B 78 03 70 49 1C 40 1C 52 1E 22 D0 8B 07 F7 D1 C3 07 14 D1 83 07 D8 D0 12 1F 12 D3 08 C9 03 80 1B 0C 43 80 00 1D 12 1F F8 D2 0A E0 08 C9 03 70 1B 0A 43 70 1B 0A 83 70 1B 0A C3 70 00 1D 12 1F F4 D2 12 1D 05 D0 0B 78 03 70 49 1C 40 1C 52 1E F9 D1 60 46 70 47 00 22 13 46 0A 46 19 46 71 B5 10 F0 03 0F 0B D0 00 2A 82 BF 00 F8 01 1B B2 F1 01 02 10 F0 03 0F F6 D1 00 2A 08 BF 71 BD 11 F0 FF 01 41 EA 01 21 04 2A 18 D3 41 EA 01 41 08 2A 0F D3 0E 46 10 2A 08 D3 0C 46 0D 46 B2 F1 0F 03 12 F0 0F 02 72 C0 10 3B FC D8 12 F0 08 0F 18 BF 42 C0 12 F0 04 0F 18 BF 40 F8 04 1B 12 F0 02 0F 18 BF 20 F8 02 1B 12 F0 01 0F 18 BF 01 70 71 BD 70 47 14 48 B0 B5 B0 F1 FF 3F 01 D0 00 F0 EB F8 12 4D 12 48 A8 42 10 D0 12 48 12 4C A0 42 0C D0 00 1B 08 3C C7 10 54 F8 08 0F 01 78 55 F8 21 20 61 68 40 1C 90 47 7F 1E F5 D1 00 F0 6D F9 0A 4D 0B 4C A5 42 05 D0 02 E0 54 F8 04 0B 80 47 A5 42 FA D1 B0 BD C0 46 FF FF FF FF 78 0C 00 00 84 0C 00 00 B0 0C 00 00 98 0C 00 00 00 00 00 00 00 00 00 00 F8 B5 84 46 40 F6 FF 74 1C F8 01 3B 00 22 10 E0 48 1B 40 1E 10 F8 01 5B 7F 1E 01 F8 01 5B F9 D1 03 E0 1C F8 01 0B 01 F8 01 0B 52 1C 5B 08 08 2A EA DA 58 08 F5 D2 1C F8 01 0B 1C F8 01 5B 05 F0 0F 07 FF 1C C5 F3 03 15 12 2F 45 EA 00 15 08 D1 1C F8 01 6B 30 0A 24 BF 1C F8 01 0B 60 F3 DF 16 BF 19 AC 42 D4 D1 F8 BD 16 49 04 28 21 D0 05 28 1A D0 06 28 13 D0 0F 28 0C D0 0F 28 1E D9 10 38 01 21 00 F0 1F 02 91 40 0F 4A 43 09 52 F8 23 00 01 60 70 47 0A 48 01 68 41 F0 01 01 F8 E7 08 46 41 6A 41 F4 80 21 08 E0 08 46 41 6A 41 F4 00 31 03 E0 08 46 41 6A 41 F4 80 31 41 62 70 47 C0 46 10 E0 00 E0 00 ED 00 E0 58 0C 00 00 4E F6 88 51 CE F2 00 01 08 68 4F F0 F0 03 40 EA 03 40 08 60 0C 48 85 46 0C 48 85 44 6F 46 07 20 87 43 BD 46 0A 48 6F 46 07 60 FF F7 4A FF 00 F0 D2 F8 00 28 01 D0 FF F7 45 FF 00 F0 75 F8 01 20 00 F0 0E F8 FE E7 C0 46 00 FE 00 20 00 02 00 00 04 01 00 20 00 BF 70 47 08 B5 FF F7 FB FF FE E7 38 B5 0D 4C 05 46 A0 68 20 B1 0C 48 B0 F1 FF 3F 00 D0 80 47 0A 48 00 68 80 47 60 68 10 B1 01 46 28 46 88 47 20 68 00 B1 80 47 06 48 00 68 80 47 FF F7 E2 FF 38 BD C0 46 E8 00 00 20 FF FF FF FF F4 00 00 20 F8 00 00 20 F8 B5 06 46 0F 4D 10 4F 73 88 00 24 17 E0 A2 00 02 EB C4 02 92 19 51 68 90 68 D2 68 52 B9 AF 42 0B D0 0A 78 55 F8 22 20 03 46 49 1C 08 46 19 46 90 47 01 E0 FF F7 66 FE 73 88 64 1C A4 B2 A3 42 E5 DC F8 BD 78 0C 00 00 84 0C 00 00 F8 B5 0B 4C 09 4B A2 68 1D 46 93 42 0A D0 A2 68 9C 46 3A 27 16 68 7F 1E 02 F1 04 02 4C F8 04 6B F8 D1 A3 60 45 F8 20 10 F8 BD C0 46 00 00 00 20 00 ED 00 E0 04 49 B1 F1 FF 3F 07 BF 00 21 08 1C 08 68 09 1D FF F7 B1 BB FF FF FF FF 02 4A 11 60 02 49 08 60 70 47 C0 46 0C 01 00 20 10 01 00 20 03 49 08 60 70 47 02 49 09 1F 08 60 70 47 70 47 F8 00 00 20 02 4A 51 68 21 EA 00 00 50 60 70 47 00 30 04 E0 02 4A 51 68 08 43 50 60 70 47 C0 46 00 30 04 E0 02 48 00 1D 00 68 00 F4 70 20 70 47 00 30 04 E0 10 B5 04 46 FF F7 AA FF 20 46 FF F7 FB FE 10 BD D0 F8 03 20 C3 1D 08 46 19 46 FF F7 FB BD 08 B5 FF F7 4C FD FF F7 20 BF 08 BD FE E7 D0 F8 03 20 08 46 00 21 FF F7 40 BE 00 21 FF F7 9D BD 01 20 70 47 70 47 00 E1 00 E0 04 E1 00 E0 01 35 00 00 04 01 00 80 DF 0B 00 33 00 19 0F C0 C6 2D 00 FF F0 00 00 00 41 0C 00 00 B1 09 00 00 25 0C 00 00 00 00 00 00 00 00 00 00 08 00 00 00 00 00 00 00 E8 00 00 00 60 0C 00 00 E8 00 00 20 88 0C 00 00 0C 01 00 20 90 0C 00 00 00 00 00 20 q
The verification-error with the bigger ti-txt-file is still there. Same call for the BSL-Scripter on the same board.
Regards,
Thomas
Thomas,
I will need to look at the specifics of the hardware invocation but I wanted to share what I have done with the SW invocation. I experimented with the BSL_PARAM but that did not make a difference. Please find the SW invocation example, the bsl script that I used, and the output log. Can you use this file to confirm that you can program via the BSL with your setup?
/* --COPYRIGHT--,BSD * Copyright (c) 2017, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * --/COPYRIGHT--*/ /******************************************************************************* * MSP432 GPIO - Input Interrupt * * Description: This example demonstrates a very simple use case of the * DriverLib GPIO APIs. P1.1 (which has a switch connected to it) is configured * as an input with interrupts enabled and P1.0 (which has an LED connected) * is configured as an output. When the switch is pressed, the LED output * is toggled. * * MSP432P401 * ------------------ * /|\| | * | | | * --|RST P1.0 |---> P1.0 LED * | | * | P1.1 |<--Toggle Switch * | | * | | * ******************************************************************************/ /* DriverLib Includes */ #include <ti/devices/msp432p4xx/driverlib/driverlib.h> /* Standard Includes */ #include <stdint.h> #include <stdbool.h> #define PORT_BUTTON_INTERRUPT (GPIO_PORT_P6) #define PIN_BUTTON_INTERRUPT (GPIO_PIN7) #define BSL_PARAM (0xFC48FFFF) //#define BSL_PARAM (0xFC48DFFF) uint8_t flag_interrupt = 0; int main(void) { /* Halting the Watchdog */ MAP_WDT_A_holdTimer(); /* Configuring P1.0 */ MAP_GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0); /* Configuring P6.7 as an input and enabling interrupts */ MAP_GPIO_setAsInputPinWithPullDownResistor(PORT_BUTTON_INTERRUPT, PIN_BUTTON_INTERRUPT); MAP_GPIO_clearInterruptFlag(PORT_BUTTON_INTERRUPT, PIN_BUTTON_INTERRUPT); MAP_GPIO_enableInterrupt(PORT_BUTTON_INTERRUPT, PIN_BUTTON_INTERRUPT); MAP_Interrupt_enableInterrupt(INT_PORT6); /* Enabling SRAM Bank Retention */ MAP_SysCtl_enableSRAMBankRetention(SYSCTL_SRAM_BANK1); /* Enabling MASTER interrupts */ MAP_Interrupt_enableMaster(); flag_interrupt = 0; /* Going to LPM3 */ while (1) { if(1==flag_interrupt) { MAP_Interrupt_disableMaster(); NVIC->ICER[0] = 0xFFFF; NVIC->ICPR[0] = 0xFFFF; NVIC->ICER[1] = 0xFFFF; NVIC->ICPR[1] = 0xFFFF; ((void (*)())BSL_ENTRY_FUNCTION)((uint32_t)BSL_PARAM); // Call the BSL with given BSL parameters } } } /* GPIO ISR */ void PORT6_IRQHandler(void) { uint32_t status; status = MAP_GPIO_getEnabledInterruptStatus(PORT_BUTTON_INTERRUPT); MAP_GPIO_clearInterruptFlag(PORT_BUTTON_INTERRUPT, status); /* Toggling the output on the LED */ if(status & PIN_BUTTON_INTERRUPT) { MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN0); flag_interrupt = 1; } /* Calling BSL */ }
// //Script example MSP432 UART BSL //Device : MSP432P401R //Comm Bridge: XDS110 - MSP432LP BackChannelUART // for this setting, the parity need to be // set from Scripter side // When MSP-BSL Rocket is used, parity will be // generated by the Rocket // //Download blink application to //MSP432 device through UART BSL // LOG MODE P4xx UART 9600 COM71 PARITY RX_PASSWORD_32 pass256_wrong.txt RX_PASSWORD_32 pass256_default.txt MASS_ERASE RX_DATA_BLOCK_32 Datenlogger.txt //RX_DATA_BLOCK_32 BSL_TEST.txt //RX_DATA_BLOCK_32 Blink_LED.hex TX_BSL_VERSION_32 TX_DATA_BLOCK_32 0x0000 0x4000 ReadBlock_cleanDevice.txt //TX_DATA_BLOCK_32 0x0000 0x4000 ReadBlock_MSP432P401R.hex REBOOT_RESET
--------------------------------------------------------- BSL Scripter 3.4.0.1 PC software for BSL programming 2018-May-17 14:13:23 --------------------------------------------------------- Input file script is : C:/MSPBSL_Scripter_win//customerRequest/script_test_01.txt MODE P4xx UART 9600 COM71 PARITY RX_PASSWORD_32 pass256_wrong.txt Read Txt File : C:\MSPBSL_Scripter_win\customerRequest\pass256_wrong.txt [ERROR_MESSAGE]BSL Password is error! RX_PASSWORD_32 pass256_default.txt Read Txt File : C:\MSPBSL_Scripter_win\customerRequest\pass256_default.txt BSL Password is correct! MASS_ERASE Mass Erase is successful! RX_DATA_BLOCK_32 Datenlogger.txt Read Txt File : C:\MSPBSL_Scripter_win\customerRequest\Datenlogger.txt Time elapsed of writing 65220 bytes : 80.41 seconds Speed of writing data :0.7921(kB/s) //RX_DATA_BLOCK_32 BSL_TEST.txt //RX_DATA_BLOCK_32 Blink_LED.hex TX_BSL_VERSION_32 Vendor:[TI] CI:[0003] API:[0006] PI:[0203] Build-ID:[0008] TX_DATA_BLOCK_32 0x0000 0x4000 ReadBlock_cleanDevice.txt Write Txt File : C:/MSPBSL_Scripter_win/customerRequest/ReadBlock_cleanDevice.txt Time elapsed of reading 16384 bytes : 20.45 seconds Speed of reading data : 0.7825(kB/s) //TX_DATA_BLOCK_32 0x0000 0x4000 ReadBlock_MSP432P401R.hex REBOOT_RESET
Regards,
Chris
Chris,
i can confirm that your code works in my enviroment. I compared it also with my code and can't find any differences, except the codesize in general and the way of invoking the bsl-launch (interrupt vs. serial command)
Did you try to flash Datenlogger.txt with BSL-Scripter in commandline-mode with verification? I tried your code with a blank device (flashed a new BSL with uniflash) and then tried to flash my software in commandline-mode. Then the verification fails and the mcu doesn't work correctly anymore. Only flashing a new BSL helps then.
I can send you the my complete project, but don't want to post it into the forum.
Regards,
Thomas
Hi Fatmawati,
i inserted 2 sections to store data and config in flash (MYCONFIG and MYDATA). This is the command-file
/****************************************************************************** * * Copyright (C) 2012 - 2017 Texas Instruments Incorporated - http://www.ti.com/ * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * * Default linker command file for Texas Instruments MSP432P401R * * File creation date: 10/13/17 * *****************************************************************************/ --retain=flashMailbox MEMORY { //MAIN (RX) : origin = 0x00000000, length = 0x00040000 MAIN (RX) : origin = 0x00000000, length = 0x0003B000 MYCONFIG (RX) : origin = 0x0003B000, length = 0x00001000 MYDATA (RX) : origin = 0x0003C000, length = 0x00004000 INFO (RX) : origin = 0x00200000, length = 0x00004000 #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 15009000 ALIAS { SRAM_CODE (RWX): origin = 0x01000000 SRAM_DATA (RW) : origin = 0x20000000 } length = 0x00010000 #else /* Hint: If the user wants to use ram functions, please observe that SRAM_CODE */ /* and SRAM_DATA memory areas are overlapping. You need to take measures to separate */ /* data from code in RAM. This is only valid for Compiler version earlier than 15.09.0.STS.*/ SRAM_CODE (RWX): origin = 0x01000000, length = 0x00010000 SRAM_DATA (RW) : origin = 0x20000000, length = 0x00010000 #endif #endif } /* The following command line options are set as part of the CCS project. */ /* If you are building using the command line, or for some reason want to */ /* define them here, you can uncomment and modify these lines as needed. */ /* If you are using CCS for building, it is probably better to make any such */ /* modifications in your CCS project and leave this file alone. */ /* */ /* A heap size of 1024 bytes is recommended when you plan to use printf() */ /* for debug output to the console window. */ /* */ /* --heap_size=1024 */ /* --stack_size=512 */ /* --library=rtsv7M4_T_le_eabi.lib */ /* Section allocation in memory */ SECTIONS { .intvecs: > 0x00000000 .text : > MAIN .const : > MAIN .cinit : > MAIN .pinit : > MAIN .init_array : > MAIN .binit : {} > MAIN .myconfig : {} > MYCONFIG .mydata : {} > MYDATA /* The following sections show the usage of the INFO flash memory */ /* INFO flash memory is intended to be used for the following */ /* device specific purposes: */ /* Flash mailbox for device security operations */ .flashMailbox : > 0x00200000 /* TLV table for device identification and characterization */ .tlvTable : > 0x00201000 /* BSL area for device bootstrap loader */ .bslArea : > 0x00202000 .vtable : > 0x20000000 .data : > SRAM_DATA .bss : > SRAM_DATA .sysmem : > SRAM_DATA .stack : > SRAM_DATA (HIGH) #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 15009000 .TI.ramfunc : {} load=MAIN, run=SRAM_CODE, table(BINIT) #endif #endif } /* Symbolic definition of the WDTCTL register for RTS */ WDTCTL_SYM = 0x4000480C;
And this are the settings in CCS
Regards,
Thomas
Thomas,
Can you give me an idea for what is the SPI configuration for your application? In the automode, the BSL will configure the UART, SPI, and I2C.
// Initialize peripheral switch(BSL432_ActivePeripheral) { case BSL432_AP_Auto: BSL432_PI_initUARTdetect(); BSL432_PI_initSPI(); BSL432_PI_initI2C(); break;
The BSL initialization of the SPI will overwrite the control register for EUSCIB0.
/** * PI initialization routine for SPI. * * Configures the SPI module and send and receive functions. * * \return None */ void BSL432_PI_initSPI() { const eUSCI_SPI_SlaveConfig BSL432_SPIConfig = { EUSCI_SPI_MSB_FIRST, EUSCI_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT, EUSCI_SPI_CLOCKPOLARITY_INACTIVITY_HIGH, EUSCI_SPI_4PIN_UCxSTE_ACTIVE_LOW }; MAP_SPI_initSlave(BSL432_SPI_MODULE, &BSL432_SPIConfig); /* Enable SPI module */ MAP_SPI_enableModule(BSL432_SPI_MODULE); MAP_SPI_registerInterrupt(BSL432_SPI_MODULE, BSL432_PI_IRQ_SPIdetect); MAP_SPI_enableInterrupt(BSL432_SPI_MODULE, EUSCI_B_SPI_RECEIVE_INTERRUPT); }
Now if there is any activity on the SPI bus, then this means that the BSL will report that IRQ_receiving.
/** * SPI interrupt routine used for detection of SPI activity. * After receiving the first byte the regular RX/TX SPI IRQ routine is registered. * * \return None */ void BSL432_PI_IRQ_SPIdetect(void) { // Interrupt status flag doesn't need to be read or reset. Reading RX buffer clears the flag. MAP_SPI_registerInterrupt(BSL432_SPI_MODULE, BSL432_PI_IRQ_SPI_RX); BSL432_RAM_RX_Buf[BSL432_MAX_BUFFER_SIZE + 5] = BSL432_AP_SPI; // Signal that SPI is PI active now uint8_t receivedData = MAP_SPI_receiveData(BSL432_SPI_MODULE); if(receivedData != 0xFF) // 0xFF is ignored. Just shifts data out { BSL432_RAM_RX_Buf[0] = receivedData; BSL432_PI_IRQ_RxDataCnt = 1; BSL432_IRQ_state = IRQ_receiving; } }
If there is SPI activity, then it would make sense that the BSL, in auto mode, would interpret this activity as a potential BSL and prevent the UART BSL from working.
Chris
Hi Chris,
i've tested with the launchpad and no external components.
This is my SPI-configuration
/* SPI Master Configuration Parameter */
const eUSCI_SPI_MasterConfig spiMasterConfig =
{
EUSCI_B_SPI_CLOCKSOURCE_SMCLK, // SMCLK Clock Source
3000000, // SMCLK = DCO = 3MHZ
500000, // SPICLK = 500khzI
EUSCI_B_SPI_MSB_FIRST, // MSB First
EUSCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT, // Phase
//EUSCI_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT, //CPHA=1
//GGf. Phase tauschen für AD7719 EUSCI_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT
EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH, // High polarity CPOL=1
//EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_LOW, // High polarity CPOL=1
//EUSCI_B_SPI_3PIN // 3Wire SPI Mode
EUSCI_B_SPI_4PIN_UCxSTE_ACTIVE_LOW|EUSCI_B_SPI_ENABLE_SIGNAL_FOR_4WIRE_SLAVE //4Wire SPI Mode
};
void spi_init(void)
{
/* Selecting P1.5 P1.6 and P1.7 in SPI mode */
MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,GPIO_PIN4, GPIO_PRIMARY_MODULE_FUNCTION);
MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,GPIO_PIN5, GPIO_PRIMARY_MODULE_FUNCTION);
MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,GPIO_PIN6, GPIO_PRIMARY_MODULE_FUNCTION);
MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,GPIO_PIN7, GPIO_PRIMARY_MODULE_FUNCTION);
/* Configuring SPI in 3wire master mode */
MAP_SPI_initMaster(EUSCI_B0_BASE, &spiMasterConfig);
/* Enable SPI module */
MAP_SPI_enableModule(EUSCI_B0_BASE);
/* Enabling interrupts */
MAP_SPI_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_SPI_RECEIVE_INTERRUPT);
MAP_SPI_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_SPI_TRANSMIT_INTERRUPT);
//RESET for ext. chip set high
MAP_GPIO_setOutputHighOnPin(GPIO_PORT_P5, GPIO_PIN0);
}
On my PCB there is one chip (Analog Devices AD7719)
Regards,
Thomas
After hours of tests and tires i found two further points an maybe the solution.
I use Timer32 in my application. After activating the timer in your Example it doesn't work anymore. When halting the timer it works again. So the start with a command over UART works now.
However the flashing failed again.
In the cmd-script i use, i send the command first and then starting the BSL_Scripter after a timeout of 2 seconds. I get the error of an incorrect header. The following code works now repeatedly:
REM @ECHO OFF
mode COM2 BAUD=9600 PARITY=n DATA=8
echo b > \\.\COM2 2>&1
mode COM2 BAUD=9600 PARITY=e DATA=8
REM wait 2 Sec
ping localhost -n 2 > nul 2>&1
c:\ti_bsl\BSL-Scripter.exe -d -g -n P4xx -i [COM2,UART,9600,PARITY] -b -z [RESET]
ping localhost -n 2 > nul 2>&1
C:\ti_bsl\BSL-Scripter.exe -d -n P4xx -i [COM2,UART,9600,PARITY] -j FAST -b -w Datenlogger.txt -v -z [RESET]
Pause
It seems that the BSL_scripter does not change the parity.
Anyway now it works to me.
The short form of the solution:
- Disable the code optimization to prevent adress-errors in TI-TXT-file
- Stop Timer32
- Disable AutoMode of Uart when using SPI for other purposes
- It works also with Scripter in Version 3.3.0
Regards,
Thomas
**Attention** This is a public forum