This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
I have leveraged off SLAA721B application report to download a BSL and custom application.
However, the application report requires a host MSP to download the application and BSL to the target MSP.
Is there a way to download the BSL and custom application without the need for a host? If so, how will this be done?
Regards
Andrew
>> However, the application report requires a host MSP to download the application and BSL to the target MSP.
The host MSP is for demo this BSL function. MSP430FRBoot on target MCU sides can be programmed through FET and IDE.
>> Which of the two BSL modes would be most appropriate for verifying a valid application?
I can't find SLA600D in TI.COM.
Based on my understanding from SLAA721B, I think that CRC checking on application validation and Dual Image Support on user code updating process should be the good option.
**Attention** This is a public forum