Part Number: MSP-EXP432E401Y
Hello,
I was trying to run the example project "tcpecho_MSP_EXP432E401Y_tirtos_ccs".
This example is supposed to print onto the console the IP Address assigned to the MSP device by the DHCP Server.
But the print is not appearing.
Then this IP Address is supposed to be used for running some python script that sends/receives tcp echo packets.
Without the IP Address of the MSP device known we cannot run the script.
Further, when the console doesn't show the IP print, then how will python script report be available on the console?
What is wrong in the example code that the console is not showing these prints?
What should I do to fully run this example application?
--
Regards,
Neeraj Sallh